Resolved! Does not generate HAL_RTCEx_SetWakeUpTimer_IT()
Code generation with STM32CubeMx version 6.5.0 is missing the HAL_RTCEx_SetWakeUpTimer_IT () that should be in the MX_RTC_Init () function.
Code generation with STM32CubeMx version 6.5.0 is missing the HAL_RTCEx_SetWakeUpTimer_IT () that should be in the MX_RTC_Init () function.
While looking at the HAL's RTC code, I noticed that in the IRQ handler for WakeUpTimer, there is no enabling of access to backup domain registers before clearing flag WUTF in RTC register ISR...Should this not be needed?When testing in my own impleme...
Hi, Just to notify a bug :CubeMX injects LL_RTC_TAMPER_MASK_TAMPER1 for RTC Tamper 2 when generating codeSTM32CubeMX - STM32 Device Configuration Tool Version: 6.8.1-RC4STMCube FW_L0 V1.12.2 /** Enable the RTC Tamper 2*/LL_RTC_TAMPER_Enable(RTC, LL_...
Hi everyone ! first time poster, hope I'm doing it right.I'm working with an STM32F107VCT and using CubeMX to generate code.I have an issue with the RTC calendar, it goes back to 0 every reset which, if I'm not mistaken, it should not on a soft reset...
Hello. I'm trying to make a code to show some menús (configuration and user menús) in a LCD screen, but something goes wrong when I try to write the year, and read it later, from the RTC calendar registers.My main code begins with the cube MX functio...
Hi,I'm using Nucleo-l476RG and try to get an Interrupt with RTC accuarcy every second.My plan is to use the RTC WakeUp in Internal WakeUp mode with "RTC wake-up interrupt through EXTI line 20"However the problem is that the interrupt is fireing only ...
The generated code in rtc.c passes zeros in GPIO_InitStruct to HAL_GPIO_Init, causing assert_param(IS_GPIO_PIN_AVAILABLE(GPIOx, (GPIO_Init->Pin))); to fail. void HAL_RTC_MspInit(RTC_HandleTypeDef* rtcHandle) { GPIO_InitTypeDef GPIO_InitStruct = ...
My code initialises the RTC using the standard CubeMX code but before setting the clock it tests for a valid year > 2018. This works perfectly and the time and date are preserved through resets of the uP. However, it appear that either the reset or t...
I think it's related to my previous question:https://community.st.com/s/question/0D53W00001sGksoSAC/is-it-possible-rtc-on-stm32h7-loses-1-second-on-each-power-cycleI applied a workaround by practically removing all MX_RTC_Init().It seems to work, how...