STM32CubeMX (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeIDE 1.15 Bug (switching from SysTick to TIM16)

I'm using the Nucleo-C031C6 board, and I chose this (NUCLEO-C031C6) from the board selector when starting the IDE. (STM32CubeIDE v1.15). I tried switching Timebase Source (in SYS menu) from SysTick to TIM16, then when I compiled, I got this error:../...

JLoh by Associate
  • 549 Views
  • 2 replies
  • 1 kudos

Resolved! Generated HAL Timer Tick generated code has an error - F7

I am using STM32CubeIDE 1.13.2 with STM32CubeMX 6.9.2-RC4.  It is an STM32F746 processor.  I'm using STM32Cube_FW_F7_V1.17.1 libraries.  I'm using Azure RTOS and selected TIM12 for the HAL tick time base.This is a side issue.  When TIM12 was selected...

tec683 by Associate III
  • 567 Views
  • 1 replies
  • 0 kudos

SysTick_Handler not called, STM32G0B1

I am using CubeIde for the first time.First test - run minimal program with HAL from CubeIDe Configurator, under debuggerSimple program, only SYSTICK and uart , but SysTick_Handler() is not trigged at all .And function HAL_Delay hangs because uwTick...

Xme by Associate II
  • 4936 Views
  • 11 replies
  • 2 kudos

Resolved! STM32F733 startup with a CubeMX project

I'm bringing up a new project using STM32F733, with code generated from CubeMX version 6.6.1, with difficulty. Looking for suggestions.1) When I change the HAL timebase source from the default SysTick to something else, I've tried TIM2 and TIM10, the...

GHolc.1 by Associate III
  • 401 Views
  • 3 replies
  • 0 kudos

Timer 6 ISR utilizing 56-60% CPU (Threadx +STM32H7)

I am using stm32h7 with threadx where TIM6 is time timebase for HAL and systick is used by threadX. The project is generated using the standard cubeMX configuration. I am using tracelyzer to visualize my CPU utilization, and i found out that TIM6 ISR...

JTari.1 by Associate II
  • 314 Views
  • 3 replies
  • 0 kudos

I2C communication in ISR

Hello everybody,     I would need to use the HAL_I2C_Master_Transmit function in an ISR, in particular I would like to use it in the HAL_ADC_ConvCpltCallback function.I have seen that the HAL_I2C_Master_Transmit function calls HAL_GetTick() so I set ...

0693W00000Ho96fQAB.png