STM32CubeMX (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem upgrading from CubeMX 6.2.0 to CubeMX 6.11.0

Hi, We have a product that is using STM32F429BIT6 processor. We've been using "CubeMX 6.2.0" and "STM32Cube_FW_F4_V1.26.1". And everything has been working fine so far. Recently, we've attempted to upgrade to CubeMX 6.11.0 and the latest FW 1.28.0 an...

VWu.1 by Associate
  • 89 Views
  • 2 replies
  • 0 kudos

STM32 LTDC image artefact (touchGFX)

Hello,My problem is now resolved but I think it can be useful to keep a trace of it for other people !I configured a project with STM32CubeMX, which uses : TouchGFX + LTDC + DMA2D with a custom 800x480 TFT Display.I was able to get an image on the di...

Resolved! Delay issues on HAL_SPI libraries

Hello everyone,  I am using SPI to communicate two Nucleo Boards (a NUCLEO-L432KC and a NUCLEO-F411RE one), and i found out a weird behavior. The idea was to perform a transaction Master -> Slave in order to select a "register" to read. Once the Slav...

vicfer89 by Associate II
  • 186 Views
  • 5 replies
  • 0 kudos

STM32F401 SPI CLK turns off with DMA

Hello Got a weird issue, to further test I created  blank project with no other code to rule out conflict. When I put in HAL_SPI_Receive_IT(&hspi3, SPI_RX_BUF, 2);,According to my logic analyzer, the clk and data pins stay high and dont move. When I ...

i-3.jpg i-2.jpg i-1.jpg i-4.jpg

Controlling Servo motors with Timers problem

I set the parameter of TIM5 of my MCU on CubeMX,the frequency of the clock is 72 MHz,PSC is 7199,ARR is 199,the information about my settings is below: TIM5 is used to output 4  channels of PWM to control four SG90 servos,TIM1 toTIM4 is used to contr...

屏幕截图 2024-03-21 183646.png 屏幕截图 2024-03-21 183735.png 屏幕截图 2024-03-21 184516.png
WINNER by Associate II
  • 271 Views
  • 4 replies
  • 1 kudos

Resolved! Error in Default CubeMX Settings for NUCLEO-F446RE

The target MCU on the NUCLEO-F446RE board receives its clock input directly from the on-board STLink-V2.1 probe (see clock signal MCO in figure below):That's because the crystal X3 is not soldered on the board by default. So, when I launch a new proj...

KristofMulier_1-1710354070214.png KristofMulier_2-1710354254259.png KristofMulier_4-1710354329998.png