STM32CubeMX (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE hangs while attempting to open .ioc file

I have intermittent problems in STM32CubeIDE 1.8.0 opening a .ioc file. When I double click on the file in the Project Explorer, I get a progress bar titled "Loading IOC". When things are working well, as soon as that bar fills up, it is replaced w...

msch by Associate III
  • 2437 Views
  • 11 replies
  • 2 kudos

LwIP + FreeRTOS not working on STM32F746

Hello folks!I have a STM32F746 MCU on my custom board and I'm trying to get the LwIP + FreeRTOS stack to work, especially the netconn tcp_echo_server example. It's not a hardware related problem, because the same HW has been used on another board (ST...

RCont.1 by Associate II
  • 716 Views
  • 10 replies
  • 0 kudos

Resolved! How to install a patch offline in the STM32Cube IDE?

in https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32cube-mcu-mpu-packages/stm32cubef4.html there are the MCU package and the patch, the first can be installed from CUBE IDE with "m...