In CubeMX, why are some chip pins shown in dashed boxes?
In CubeMX, why are some chip pins shown in dashed boxes?
In CubeMX, why are some chip pins shown in dashed boxes?
Hi guys!Still live and kicking, thanks God! My fist public version was/is vscode_nucelo_l152re (totally uninspired, I am bad with naming things) that is a visual configuration tool for the Nucleo_L152RE board and generates code that uses the old SPL ...
Hello,I'm having trouble with ADC2 and ADC3 on my NUCLEO-L010RB board. I've utilized all 16 ADCs on the microcontroller, and the code is functioning correctly except for these two ADCs. I am using LPUART.In this image, I obtained a reading of 40 from...
Encountered an annoying project generation bug recently. By default CubeMX adds to keil project a hwhole bunch of files:Even if you don't need any of the LL. So, when you tick "Enable Full Assert" checkbox, it causes an error, because no "stm32_asser...
Hello All,I am using the STM32L011K4 to control the PWM duty cycle through the use of the DMA.I have gone through my register initialization to ensure that the registers are being configured correctly and I have gone through and used the solution fro...
Hello,I am trying to figure out what is the version of the LL drivers used in a project. Where can I find this information, is it stated in any header file? I could not find anything so far.Thanks in advance!Andreea
I use STM32CubeMX and Keil MDKI generate code and open project , but only open project.eww..-.
Hi, Just to notify a bug :CubeMX injects LL_RTC_TAMPER_MASK_TAMPER1 for RTC Tamper 2 when generating codeSTM32CubeMX - STM32 Device Configuration Tool Version: 6.8.1-RC4STMCube FW_L0 V1.12.2 /** Enable the RTC Tamper 2*/LL_RTC_TAMPER_Enable(RTC, LL_...
Hello, I'd like to better understand some settings in CubeMX to be sure default settings are OK for my application.Starting with USART2 Configuration for example:- in "DMA Settings" tab, what behavior is modified by the Priority dropdown (Low, Medium...
Hello, I've got problem with STMCubeIDE. You can see my problem at photos I attached. Can anyone help me to solve this problem. I try to work on Lenovo Legion 5 with Ryzen 5 5600h and RTX3060. Second graphic card is integrated with Ryzen CPU. This pr...