STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Strangely accurate ADC noise

I've been struggling with a strange ADC problem for a while, and have now made some interesting observations.The scenarioI'm using an STM32G474, where HRTIM directly controls a peltier driver for temperature regulation. Temperatures are measured by A...

Big chart 1.png 83F - 1.png 73F - 1.png 7BF - 1.png
EThom.3 by Senior II
  • 37 Views
  • 4 replies
  • 0 kudos

STM32G4 UART Signal Handler Error

Hi there, I have firmware that uses UART1 and UART2 of the STM32G4 series. Both are intended to run on interrupts, but as soon as any signal is received by the MCU, an error occurs, causing HAL_UART_AbortCpltCallback to be called. Therafter, the inte...

Clipped sine TCXO clock for STM32G031G8U6

The STM32G031G8U6 in a UFQFPN28 package does not have PF0 / PF1 pins for HSE OSC_IN / OSC_OUT.  It does however have OSC_IN on PC14.  This is intended for an external CMOS oscillator in bypass mode.I’m currently in the schematic design stage. My boar...

BK1 by Associate II
  • 275 Views
  • 5 replies
  • 0 kudos

STM32U575CGU3 CAN Cycle Time Issue

I am using the STM32U575CGU3 MCU in my project, where I transmit data using two CAN frames on the bus. I have configured a CAN transmission cycle time of 250 ms in my software. However, on a few PCB assemblies, I am observing inconsistencies in the ...

STM32F4 + DP83848: Ethernet not working

I am a beginner in electronics. I recently designed a board using the STM32F407VGT6 and DP83848, but after assembly and testing, I encountered a problem.  The board can be programmed and it runs, but the Ethernet section does not work properly.  It d...