STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407 write protected on chip

Hi folks, i have an STM32F407 discovery board. when i measure the voltage across the gpio pins it becomes write protected. after i dumped many codes but no use. i had attached the screenshot with the error code that it's display. i tried to put jum...

0690X000006C6OVQA0.png 0690X000006C6OQQA0.png
Ark1 by Associate II
  • 2674 Views
  • 5 replies
  • 0 kudos

I2C problem in reading VCNL 4040 proximity sensor

Hi,I got the VCNL4040 Proximity sensor breakout board. I tried this board with Arduino Uno example solution and works very well.Now, I am trying to read this sensor with an STM32L0 series MCU. I see I am able to write to the sensor by turning ON and ...

ashah.16 by Associate II
  • 3532 Views
  • 2 replies
  • 0 kudos

Resolved! Can't reset the core

Hi,When attempting to connect to an STM32F030C8T6 MCU, ST-LINK Utility gives the following error message:"Can not connect to target!If you're trying to connect to an STM32W1xx device, please select Normal or HotPlug mode from Target->Settings menu.If...

JS8 by Senior
  • 4658 Views
  • 5 replies
  • 0 kudos

Resolved! is it possible to log data in internal flash?

Hii everyone,I am facing the problem for the data logging in flash.i am not able to keep track of the variable till where the flash memory is filled is there any way to sort out this problem. i am not able to erase the single word to update the addre...

Resolved! USB on STM32G0

I developed a user device with a STM32G030 in it. Now I want to go to the market. But before that, I want to have a USB port on my board with which users can update their firmware in case my software has bugs. In the STM32G0x0 datasheet (RM0454) in c...

JanAtze by Associate II
  • 4354 Views
  • 4 replies
  • 1 kudos

nucleu-h745zi-q rs485 without external module

Hello//   nucleu-h745zi-qI want to use hardware flow control rs485Previously, i used an external module because there was only rs232 (f103).** question ** . With this feature, can the module be removed and the microcontroller directly connected to A ...

MGH745 by Associate II
  • 2034 Views
  • 4 replies
  • 1 kudos

Resolved! Why does LwIP need CPU DCache (on STM32H743)?

To enable LwIP in CubeMX (inside CubeIDE) it needs the CPU data cache enabled.  Ok, no problems, but it doesn't explain why and I can't find why this is the case. Is anyone able to offer an explaination?  

musmuris by Associate II
  • 6199 Views
  • 9 replies
  • 3 kudos