STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f779i -EVAL IAP

Hello experts,I am using stm32f779I - EVAL evaluation kit, am trying to implement LWIP IAP on this board for that I have used example code from the repository C:\Users\Aravind\STM32Cube\Repository\STM32Cube_FW_F7_V1.17.0\Projects\STM32F769I_EVAL\Appl...

Aravind1 by Associate II
  • 1594 Views
  • 2 replies
  • 0 kudos

UVC+CDC USB Composite device on STM32F411

Posted on August 01, 2016 at 16:02 Overall objective: Using https://github.com/groupgets/purethermal1-firmware as a base, add a USB serial port interface (which would replace the DEBUG functionality it has currently). I have read thro...

Resolved! STM32 SPI communication Master issue

Recently working with spi communication in stm32g070rb using stm32CubeIDE (HAL library).SPI master receive interrupt triggered continuosly when there is no interrupt.But same code wrote in SPI slave its works perfectly.I also put Pull down resistor.P...

vignesh1 by Associate III
  • 3300 Views
  • 5 replies
  • 0 kudos

STM32U5 HAL_Delay block

Hello,I met a HAL_Delay() block. The board worked with internal RCC, and I checked the uwTickFreq when debugging, it always equal to 0.  Attached the ioc file. 

lilyGUO by Associate II
  • 2668 Views
  • 5 replies
  • 0 kudos

STM32WB55 Nucleo with IMU (LSM6DSV16X) HAL_ERROR

Running into a weird issue with my teams and I's capstone senior project. We are using the Nucleo dev boards and connecting it to IMU in the title via I2C. When running either HAL_I2C_Mem_Read or HAL_I2C_IsDeviceReady the status we get back is HAL_ER...

JJcompE by Associate
  • 1074 Views
  • 2 replies
  • 0 kudos

Erase - unlock STM32L083

I am using STM32L083 and need to erase it using J-Link. If it is locked at Level1, I also need to unlock it. My goal is to completely erase the entire Flash memory. I believe I have an error in the process, as I have been unsuccessful in both erasing...

JR2963 by Senior II
  • 2092 Views
  • 0 replies
  • 0 kudos

Resolved! Can the STM32H7x M4 core boot from SDRAM or not ?

According to the STM32H7's datasheet, the M4 core shouldn't be able to boot from an SDRAM memory address (because it's outside of the range 0x00000000 to 0x3FFF0000):However, I found out that I can actually boot the M4 core from SDRAM, if I used the ...

IbrahimAbdalkader_0-1705573213089.png