User Activity

Hi ,   I made a STM32F405VGT6 board with SD card interface. The SD code is generated using STM32CUBEMX and FatFs middleware.   The SD file write is not stable, it return error sometimes after calling f_write(). However, if I run the same code in uVis...
We connect STLINK/V2 to STM32G071 with 3 wires : SWDIO, SWCLK and GND. It always failed to connect. However, we can connect by using JLINK. We notice that STM32G071 combines the boot0 with SWCLK. Does this make STLINK/V2 failed to connect ? How can w...
I need to develop a bootloader on STM32L476. So I adapt my code from this tutorial and codes : video https://www.youtube.com/watch?v=OkUQ3iMmiYQ&list=PLnMKNibPkDnEb1sphpdFJ3bR9dNy7S6mO using STM32G071 , However, my adapted code running on STM32L476 a...
It seems there is a mistake in STM32Cube\Repository\STM32Cube_FW_L4_V1.13.0\Projects\STM32L4R9I-EVAL\Examples\OSPI\OSPI_NOR_MemoryMapped project, the STM32L4R9I-EVAL board flash chip is connected in OCTOSPI1, but in this project, the instance is OSPI...
Kudos from