STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SD Card

Posted on March 30, 2017 at 18:49Hi, I'm using the cubeF4 to work on FATFS application and i'm searching for a function in FATFS library that can return the content of the SD Card: number of files and their names.  Thank you.

nechi by Associate III
  • 4210 Views
  • 9 replies
  • 0 kudos

Resolved! STM32F217 HSE and Timer Sync

I'm working with an STM32F217 and I have a few timer channels setup as sync clocks to regulators (around 1.5 MHz). I'm checking to make sure my sync lines are actually using HSE as a reference clock by looking at the phase drift between my external o...

PCarn.1 by Associate III
  • 5896 Views
  • 12 replies
  • 1 kudos

Resolved! SIL 2/SIL 3 Microcontroller requirement

hiwe have requirement of SIL2/ SIL3 verified microcontroller which have 24 adc channel, UART(2), ETHERNET, CAN(2),SPI,I2C, 512KB FLASH ETC.kindly suggest us 

Singh_t by Associate II
  • 4186 Views
  • 2 replies
  • 1 kudos

disable debug in low power mode (sleep mode) in stm32u575

hello ,I am looking for disable debug in lower mode in stm32u575 MCU as they  have option to disable  debug mode in low power mode like "STOP 1 2 3 " but not available for low power sleep mode is there any  one have worked on it and dose it have some...

PESHWA by Associate II
  • 1993 Views
  • 1 replies
  • 0 kudos

Resolved! product recommendation for patient monitor

Hi, I am seeking product recommendations from you for developing our project using an NXP board. We require a simple and cost-efficient board suitable for a medical patient monitor. Key considerations include interfacing with a 12-lead ECG module (SP...

TIM1 break interrupt not firing

Hi,I am configuring TIM1 to generate interrupt via MX and I can see that the ISR for TIM1 break is added to the code.But the interrupt never triggers. I know that break from comparator does happen, but no interrupt!Does anyone know what could be wron...

bolurian by Associate II
  • 3250 Views
  • 5 replies
  • 1 kudos

Resolved! Multi Channel ADC with DMA transfer on NUCLEO U575ZI-Q

Hello, I'm trying to configure my NUCLEO-U575ZI-Q to read multiple channels of ADC at once. I will describe the settings in the following and then raise my questions:1- I use IN1 and IN2 on ADC4 which corresponds to PC0 and PC1 on the EVB2- I set sca...

mebrahim by Associate II
  • 8760 Views
  • 9 replies
  • 1 kudos