User Activity

Hello ST community,I am unfortunately facing a problem with the MP34DT05-A MEMS microphone. I am using the DFSDM module to read in the microphone. Unfortunately, it happens again and again that extremely strong noise is added at a random time (see pi...
Hello,i am currently working with MATLAB/Simulink and followed this tutorial: https://www.youtube.com/watch?v=535gxJa72v0.When I tried to bring the Pulse Generator to its maximum with Digital Write, surprisingly it already stopped at 25kHz. After som...
Hello ST Community,i am currently working with MATLAB/Simulink and STM32 Nucleo Boards. Now i am facing a problem: I want to use "Run on Hardware Board" using "STM32L4xx Based" option in Simulink model settings. However, since i have to work offline,...
Hello st-community,I am currently working with MEMS microphones (more precisely: MP34DT05TR-A). For reading in the data I use the DFSDM, which also works as far as possible, because I noticed when evaluating the data using an FFT that there is a very...
Hello,the STEVAL-MIC007V1 with the IMP23ABSU is on the first sight quiet interesting with the microphone bandwith up to 80kHz. However (due to imprecise reading from me) it turned out that this is a analog MEMS microphone. The STEVAL-MIC001V1 with th...
Kudos from