STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H745 SPI Cores communicating

Hi!I'm using STM32H745 dual core. The reason behind it is as I have to do very fast measurement on one core (M7) and the rest of the slower things on the M4. The M4 is mostly used for communicating with the external world. I have setup SPI3 and SPI4....

__silardg by Associate III
  • 6977 Views
  • 13 replies
  • 0 kudos

ADC multimode DMA init error

I am using ADC regular simultaneous mode with stm32f427It works nice with the pulse signal is comming after dma start(HAL_ADCEx_MultiModeStart_DMA)but if the signal is comming before calling ADC dma start code it going to infinityhow to solve this?i ...

SKim1761_0-1707793855535.png
SKim.1761 by Associate III
  • 1031 Views
  • 0 replies
  • 0 kudos

STM32H7 TIM12 TRGO DAC DMA syncronization

Hello,I am trying to generate a pulse-triggered waveform continuously by using DAC and DMA in STM32H735RGV6. To do this, I have opened DAC OUT1 with the following configuration.After that, I set up the TIM12 with the following configuration and expec...

ErsinKuscu_0-1707732708749.png

Resolved! Stm32f410RBT6

Hello, we are a manufacturer company that uses STM products. We developed a device using stm32f410 and stm32f446 products 2 years ago. We have a few processors from this old series, stm32f410 and stm32f446, and they work without any problems. However...

TIM1 counting pulse from input signal help

Hello, I currently have a test bench project to carry out, so it's a drive motor that turns another motor, which generates an FCEM signal on my 3 phases, but the duration of the signal depends on the speed at which I'm turning, so I'd like to use tim...

spislave.png

Resolved! STM32G473 datasheet - upper limit on ADC external trigger period

Hi,maybe I don't know how/where to look, but I can't find any info why in datasheet for STM32G473 there is the max value for T_trig (external trigger period) in ADC timing characteristics (see the attached image). I several datasheets for several oth...

hepoun by Associate II
  • 4525 Views
  • 6 replies
  • 1 kudos

Resolved! Environmental Impact of manufacturing STM32

Hello everyone,  I have a bunch of questions concerning the environmental impact of manufacturing a STM32  I'd like to see the impact according to as many criteria as possible from the following:  Contribution to the greenhouse effect Particulate mat...

Chall24 by Associate II
  • 5520 Views
  • 10 replies
  • 1 kudos

Resolved! Connecting Arduino Portenta H7 to PDM microphone

Hello everyone,I am new to hardware programming so please excuse my basic question. Can someone please point me to the right resource to obtain data from an external pdm microphone (https://learn.adafruit.com/adafruit-pdm-microphone-breakout?view=all...

yshetty by Associate II
  • 3370 Views
  • 4 replies
  • 1 kudos