HelloI want to update my variable continuously on Memory, so whenever bootup and power loss I can read that Value.So which is the best way to store variable and read when MCU bootup.
how to read 600 K(6 Lakh ) and more character at a time using Fat FS Micro SD Card , my File store in SD Card in File more then 6 Lakh Character is there , If any other way to read please help me , thanks in advance
Yes i checked the File length using f_size in my file 650000 length, when i am read the file using f_read then hard fault error is there. Buffer data type is BYTE.I need the whole file character in one buffer,i mean 650000 character.