STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U5[Ax] Usb Host Multi-Packet Data Toggling

Hi all, I am not able to fully understand how the DATA0/DATA1 toggling works when performing multi-packets transmissions. For "multi-packet" transmission I mean that the "num_packets" in USB_OTG_HCTSIZ_PKTCNT register is greater than 1, (i.e. I want ...

bluluiss by Associate II
  • 2021 Views
  • 3 replies
  • 0 kudos

Resolved! Automatically entering and exiting bootloader

Is there a way to make STM32Cube Programmer controls a pair of pins in a CH340 or similar USB to TTL converter, to be able to control BOOT0 and NRST pins of an StM32 micro? I would like to make  a simple circuit that permits entering and exiting a bo...

Castelo by Associate II
  • 1822 Views
  • 1 replies
  • 1 kudos

Resolved! STM32H7A3 I2C_CR1 bit NOSTRETCH settings

Currently try to configurate settings for register I2C_CRI. Not sure which value should I set for bit NOSTRETCH. I am using I2C as master. This bit only effected when using I2C as slave. But in manual mention must kept cleared in master mode.  Meanin...

NRAML.1 by Associate II
  • 3082 Views
  • 2 replies
  • 0 kudos

Resolved! High current draw Vbat Bluepill

Hi,This is the first time I am starting a post, sorry in advance if it's not in the correct place.I have a Blue-Pill with original STM32F103C8T6. I have Vbat hooked up to a 0.33 F super cap via 100 ohm. Vdd is connected to V bat with a BAT54C Schottk...

NLHL by Associate
  • 5953 Views
  • 5 replies
  • 3 kudos

MDMA Block transfer only transfers one block

Hi all, i am trying to use MDMA to transfer data from a cyclic ADC-DMA buffermy ADC buffer is of x size and it is cyclic: adc_buffer[x]and i want to transfer its data via MDMA to a larger buffer while its samplingmeaning that after every ADC iteratio...

shahaf321_0-1708006211819.png shahaf321_1-1708006643985.png
shahaf321 by Associate III
  • 985 Views
  • 0 replies
  • 0 kudos

Resolved! How to use SD card and eMMC together in STM32H7

안녕.최근에 STM32H753XI를 사용하여 맞춤형 보드를 만들었습니다.보드의 초기 테스트를 위해 각 주변 장치에 대한 테스트를 실행하고 있습니다. 대부분의 경우 잘 작동하지만 SD 및 eMMC 사용에 문제가 있습니다.내 보드에는 SD 슬롯 1개와 eMMC가 포함되어 있습니다.eMMC는 SDMMC1에 연결되고 SD는 SDMMC2에 연결됩니다.그리고 둘 다 FatFS에 연결하여 파일 시스템으로 사용합니다.둘 다 각각 사용할 때 매우 잘 작동합니다...

SDIO_sch.png eMMC_sch.png CORETEX_M7.png NVIC.png

Resolved! Mismatch of DTCM-RAM cache attribute in documentation

In Figure 1 of the reference manual RM0433 for the STM32H743 (and STM32H742, STM32H753, STM32H750) no connection between cache and DTCM-RAM exists.  For all I know this is correct since the DTCM-RAM is not cachable.Table 7 on the other hand shows tha...

dmocom_0-1707908626572.png dmocom_1-1707908975086.png
dmocom by Associate II
  • 3399 Views
  • 4 replies
  • 4 kudos

Resolved! STM32u5a9 hexa-spi PSRAM issue

I am attempting to bring up a custom board using a STM32U5A9 chip. I modeled the board off of the STM32u5a9j-dk dev kit (the one with a circular screen). I've been able to get our LCD screen to work over DSI and touchGFX currently runs fine.Now I am ...

nwm_35 by Associate III
  • 8025 Views
  • 10 replies
  • 0 kudos