Hi! Can you recommend me a suitable usb driver to connect STM32H735VGH in device mode ?And please suggest me if any additional configuration required to work with.Thank you.
I'm configuring STM32H735VGH MCU for communicating by USB_OTG full speed, Device mode and want to power it by VBUS.Suggest me best whether power distribution switch is required or not ?
Hi! I am using STM32H725VGH6 series MCU, in the datasheet it is clearly mentioned that it has 2 direct 16bit ADC channels, while it is not there when trying to configure in STM32CubeIDE. Can you make sure the datasheet is correct or not?
Here I've attached a snapshot (datasheet STM32H725xE/G, page n. 20), mentioned number of direct channels ADC1/ADC2 is 2. Can you please confirm me the MCU pins (pin number/name which can be configured for these channels) for these channels?
Can you please go to my main question mentioned below-I am using STM32H725VGH6 series MCU, in the datasheet it is clearly mentioned that it has 2 direct 16bit ADC channels, while it is not there when trying to configure in STM32CubeIDE. Can you make...
This became helpful for understanding the interleaved mode configuration of mcu, but here I want configure as differential (not single ended), interleaved mode using direct channel ADCs so that it can be achieved high sampling rate. So please help m...