Skip to main content
Associate
April 25, 2025
Question

question about STM32G474 dual banks

  • April 25, 2025
  • 4 replies
  • 735 views

I have a test question about STM32G474 dual banks to ask :
A test program for LED flashing has been successfully constructed in the IAR environment.
Use STM32CubeProgrammer to load BANK1 starting from 0X8000000, DBANK=1,BFB2=0, and the program runs OK
When BANK2 starting from 0x8040000 is loaded, DBANK=1 and BFB2=1, the program cannot run
May I ask to see if there are any problems with my application Settings

thank you

This topic has been closed for replies.

4 replies

mƎALLEm
ST Technical Moderator
April 25, 2025

Hello,

Look at the example provided in the STM32G4 Cube package especially the example FLASH_DualBoot located at this Github link.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate
April 25, 2025

Thank you
Yes, I have referred to this program
Now I'm just verifying the deployment of the firmware in a manual way. Later, the program switching process will be placed in the program (my application is digital power firmware deployment and upgrade).
The firmware is fine when deployed on BANK1, but not on BANK2.
This is exactly what I want to consult.
You can also have a try.
Thank you for your reply

Associate
April 25, 2025

the process below:

微信图片_20250425193045.png微信图片_20250425193143.png微信图片_20250425193211.png微信图片_20250425193232.png微信图片_20250425193255.png微信图片_20250425193314.png微信图片_20250425193350.png

 

Senior
May 3, 2025

Both banks will be swapped with BFB2=1 and all addresses from BANK2 will be remapped to BANK1 (and vice versa).

Otherwise the flash addresses, generated by compiler, would all be wrong. So the start address for booting from BANK1 (BFB2=0) and from BANK2 (BFB2=1) also stays the same virtually @0x08000000.

If you want to ask if you booting from BANK1 or BANK2 you can read the memory remap status in MEMRMP register:

DWORD GetBootBank(void)
{
 return (READ_BIT(SYSCFG->MEMRMP, SYSCFG_MEMRMP_FB_MODE) == 0) ? FLASH_BANK_1 : FLASH_BANK_2;
}