STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G473QET6 Dual Bank/Boot Mode Question

I am having some issues implementing dual bank/boot.I have set up a dummy project starting at base address 0x08000000 for 256k bytes that will turn on a red LEDI have another dummy project starting at base address 0x08040000 for 256k bytes that will ...

kip18 by Associate III
  • 1731 Views
  • 1 replies
  • 0 kudos

Resolved! NUCLEO-L4A6ZG Board/ST-Link not recognized

After about an month, I connected my NUCLEO-L4A6ZG to my PC again. STM32CubeIDE nor the STM32CubeProgrammer can't recognize my board. I already tried different USB ports and different USB cables.When Trying to run a program the Error Message in the I...

stmax_0-1708545446608.png
stmax by Associate II
  • 1742 Views
  • 2 replies
  • 1 kudos

SPI Send (sizeof) too big

Hi, I am wondering if anyone has any experience with HAL SPI as when I try in 16-bit mode to make a single packet of data manually and use (sizeof xxx) it sends 2x data packets to the oscilloscope and when I specify the packet size as "1" I get the c...

PLee.3 by Associate III
  • 4552 Views
  • 6 replies
  • 2 kudos

Resolved! STM32H750VBT HRTIM not working

I cant make work the HRTIM. I am using the weact board.I tried HRTIM-A and TRTIM-D using the cubeide (latest updated). the first one using "basic HAL" and the second using "Advanced Hal" instructionsTIM5 works so it seems that clock is working.I adde...

Advanced.jpg Basic.jpg Master.jpg
JLope.11 by Associate III
  • 1446 Views
  • 1 replies
  • 0 kudos

Resolved! LPTIM not counting down in encoder mode, always counts up (G071)

I have an STM32G071CBTx with a rotary encoder wired to GPIO pins PB5 + PB7 (LPTIM1_IN1 and LPTIM1_IN2), but for some reason it will never count down no matter which way the encoder is turned.I have checked the encoder waveforms and they are as expect...

JU by Senior
  • 2268 Views
  • 1 replies
  • 0 kudos

TIM Output compare on STM32F407

Good morning community,I am trying to capture output compare unit.Board: STM32F407G Discovery.I configure TIM1 which is 16bit timer on bus1.Reference clock is 12.5Mhz in our case.I am seeing when I run the code only one time interrupt is generated an...

MG1 by Associate II
  • 17516 Views
  • 3 replies
  • 0 kudos