User Activity

Hello Community, I have been working in an app that has 2 different lenguages defined in the "Texts" option in TouchGFX. In the Canvans i have for example a textArea that is configured as "Auto-size" with typography "Large, 40px" and centered alignme...
Hello community! I am developing an app that is running in an H7 MCU, the M7 core app is "turning on" the M4 and then is running to an external flash where is the actual M7 code.I am looking to implement an update in this M7 "bootloader". As i unders...
Hello,  I am trying to install FileX + LevelX in an stm32h7 microcontroller using a nor custom driver. I do have in my hardware an AT45DB641 NOR memory. I am working it as an stand alone and also with fault tolerant enable. My flash chip does have 40...
Hello community,I am working on a project that involves the use of both CM7+CM4 cores from an stm32h7, to communicate both i need to use openamp. I have successfully made an standalone project that only have the openamp working, but when i port it to...
Hello,I have been working in a project with the mentioned MCU and by now i have been working it with SMPS_SUPPLY and VOS3 to work at 100Mhz Both CM7 and CM4.By now days i need to boost it up to 400Mhz and 200Mhz, so i need to change from VOS3 to VOS1...