cancel
Showing results for 
Search instead for 
Did you mean: 

If the bootloader will enter system ROM bootstrap first when using flash mode to boot in stm32f103

yjlong
Associate

When I downloaded applicaton into flash, I found that it will respond my cmd code if I send cmd code immediately after NRST changing from 0 to 1.

If although I choose  'Boot0(pin) = 1和Boot1(pin) = 0' to flash mode, the stm32f103 will also enter system rom bootstrap code.

It's to say that stm32f103 entering flash mode is bypassing System Rom Bootstrap code.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0