STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! pwm ws2812 not workin

Hi! i am doing example pwm ws2812 with dma, configure the time 1 with ARR=60, using clock= 48 mhz, my pwm not working full buffer i don´t know why not work full buffer, the pwm have 12 pulse, i am sending for one led ws2812 is 24 pulse./* USER CODE ...

0693W00000WKvAGQA1.png
jdo by Associate II
  • 3791 Views
  • 8 replies
  • 0 kudos

Resolved! SWO stops collecting data after a few packets

I'm trying to do some debugging using SWO on an STM32G474. After a very short amount of time no new packets are displayed in CubeIDE (usually after ~2500 packets). I limited the SWO frequency to various values between 100kHz and 8 MHz. Using an oscil...

Herm by Associate III
  • 7069 Views
  • 13 replies
  • 2 kudos

Resolved! PWM in Stop2-Mode with LPTIM2

Hello,I am using STM32U575 and would like toimplement a PWM output. This should also work in Stop2-Mode.Clock for the LPTIM is LSE. It works with LPTIM1 and 3 without any problems.To generate a PWM in Stop2-mode, I use the LPBAM with LPDMA. Now I wou...

JoachimO by Associate II
  • 3074 Views
  • 5 replies
  • 4 kudos

Resolved! possible errata in STM32L4R5 reference manual (rev9)

page 1320; timer 2 input pwm mode"1. Select the active input for TIMx_CCR1: write the CC1S bits to 01 in the TIMx_CCMR1 register (TI1 selected).2. Select the active polarity for TI1FP1 (used both for capture in TIMx_CCR1 and counter clear): write the...

b.a. by Associate III
  • 2007 Views
  • 3 replies
  • 0 kudos

Program option bytes safely in STM32 MCU | STM32G041F6P6

I aim to set the IWDG (Independent Watchdog) to STANDBY mode to ensure that our MCU remains in that state without being awakened by the Watchdog. To achieve this, I utilized the following command with STM32_Programmer_CLI.exe:After executing the comm...

How do I get STM32F0 to show up under "Ports " in device manager?

My STM32F0 won't show up under "Ports " in my device manager. It does, however, show up under "Universal Serial Bus Devices". I'm trying to print to a serial monitor. I've spent over 12 hours (low guess) trying to troubleshoot this issue. Here is wh...

0693W00000KbNFGQA3.png 0693W00000KbNGBQA3.png 0693W00000KbNGaQAN.png 0693W00000KbNGGQA3.png
CR72 by Associate II
  • 11899 Views
  • 17 replies
  • 0 kudos

Resolved! Errors in figure

In RM0351 Reference manual Figure 420. USART block diagram, the positions of shift registers and data registers (of both Transmit and Receive) are wrong; their positions should be swapped.  

errors_in_figure.png