Skip to main content
Asantos
Associate III
July 26, 2023
Solved

STM32H573VI ETH_TXD1 and ETH_TX_EN pins

  • July 26, 2023
  • 2 replies
  • 1500 views

Hi,

When using the STM32CubeMX to configure the ethernet pins for the STM32H573VI, the TXD1 and TX_EN pins can be configured to the PB13 and PB14 pins. But the STM32CubeMX does not allow these pins to be configured for ethernet for the STM32H563VI. In the datasheet of both, PB13 and PB14 cannot be configured for ethernet. I wonder if PB13 and PB14 really cannot be configured for ethernet?

This topic has been closed for replies.
Best answer by Ghofrane GSOURI

Hello @Asantos 

Thank you for your contributions and for your detailed explanations,

I confirm the issue on my side, it has been reported to STM32CubeMX development team .

Internal ticket number:158178(This is an internal tracking number and is not accessible or usable by customers).I will keep you posted with updates.

Thx

Ghofrane

 

2 replies

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
July 27, 2023

Hello @Asantos 

Thank you for your contributions and for your detailed explanations,

I confirm the issue on my side, it has been reported to STM32CubeMX development team .

Internal ticket number:158178(This is an internal tracking number and is not accessible or usable by customers).I will keep you posted with updates.

Thx

Ghofrane

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Amel NASRI
ST Technical Moderator
November 30, 2023

Issue fixed since STM32CubeMX 6.9.2.

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.