STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FIT / MTBF values needed

Hello,I need the FIT values / MTBF values from the following parts:- STM32F105x- STM32G474x- STM32F303x

WHU by Associate
  • 1669 Views
  • 3 replies
  • 2 kudos

Turn off pll before entering sleep - STM32F410RB

Hello,i am using stm32f410rb device, where i want to do some things at 100mhz using HSI only, and pll.After this i am puting the device in sleep mode, and  provide wakeup using the rtc interupt.The HSE is not used. My problem is that before sending t...

Bogdan by Senior
  • 2658 Views
  • 3 replies
  • 3 kudos

Resolved! PWM No Output for TIM1 on STM32L476

I use Cube to setup TIM1_CH4 on PE14 as PWMSetup of iocPE14 -> TIM1_CH4 in pinoutTIM1:Ch 4 PWM Generation Ch4Conter Settings: Counter period 20PQM Generation Cannel 4: Pulse 5Modification of main:/* USER CODE BEGIN 2 */HAL_TIM_PWM_Start(&htim1, TIM_C...

PeterL by Associate III
  • 7038 Views
  • 7 replies
  • 1 kudos

Resolved! STM32 PKA RSA Montgomery Parameter

The PKA peripheral can precompte the montgomery parameter, which is documented as "R2 mod n". If I compute this offline with R being the normal (2 ^ b) [b the numbers of bits in the modulus n], I am getting a different result than what PKA computes. ...

STM32L496 LED problem

Hello everyone! Currently I'm working in STM32L496ZG-p Nucleo board, I have written code for both MCU specific header file and Driver specific header file and I started to build a simple project to make a LED blink. But I haven't got the proper resul...

Ratheesh by Associate
  • 1393 Views
  • 2 replies
  • 1 kudos

UART CTS signal stuck at high after framing error

Hi all.We are using a bidirectional UART with hardware-flow control lines (RTS/CTS) between two microcontrollers.One of the controllers (A) is an STM32H7, the other controller's type (B) should not be relevant. I write this from the perspective of A....

mwb_1-1711018482094.png mwb_2-1711018639890.png mwb_3-1711018737948.png mwb_4-1711019070363.png
mwb by Associate III
  • 1571 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F407 TIM2 DMA driving neopixels

I have been reading a bit about neopixels and the communication protocol they work. I have been searching for a library for the WS2812B neopixel but could not find one that would work out of the box hence I have decided to write my own neopixel drive...

LPetr1_0-1709548050591.png LPetr1_1-1709548127989.png LPetr1_2-1709548146112.png LPetr1_3-1709548456479.png
LPetr.1 by Senior II
  • 10654 Views
  • 11 replies
  • 2 kudos