User Activity

 Hi @Peter BENSCH  I have a query regarding voltage compatibility of Quad single-pole single-throw analog switch from Nexperia 74HCT4066.The switch part is voltage compatible with STM32G431MB/ME series when analyzing VOH VIH VIL VOL relationships wit...
Hi Team, @Peter BENSCH  I want to process PWM HART signals of 1.2 KHz/2.2KHz. Will the op-amp TSX631A be suitable for this application which is having a bandwidth of 200 KHz?  Regards,Sreejith R Nair
Hi,@Peter BENSCH In the datasheet of ST LMV321ILT op-amp, it is stated that minimum voltage supply span is 2.7V and maximum supply span is 6V. Can you suggest whether LMV321ILT can be used with 3.3V or an alternate that is both pin to pin and 3.3V co...
Hi, Greetings @Peter BENSCH  I am using STM32G431MB controller in my project. I am configuring PB4 as my General purpose Input pin. Ports PB5-PB9 as well as PC8,PC9, PA8 and PA9 are assigned as General purpose outputs connected to Analog HART Mux. In...
Hi Team, @Peter BENSCH  We  are currently using ST Micro controller STM32G431MBT6 on our project.   We are shorting the following pin combinations for HART output feedback which serves as an input to the HART Out generator: PC15(Pin4) and PC0 (Pin8);...
Kudos from
Kudos given to