STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE unable to debug

I am using the STM32F746 board and trying to program the microcontroller. However, the STM32Cube IDE software is showing an error, as shown in the figure. The "stlink_USB" and "5V" are connected.

USEF_k by Associate II
  • 3728 Views
  • 5 replies
  • 0 kudos

SAI transmission to external DAC - more serial data outputs ?

Hello dear community,I’m working on a USB sound interface, using a STM32F7 and an external DAC chip offering 8 stereo output channels.Most of the DAC are offering multiple serial data inputs ports. For example, the Analog Device ADAU1966A is offering...

sai.png
jean by Senior
  • 1674 Views
  • 0 replies
  • 0 kudos

Interfacing With STM32G474E-EVAL1 SDRAM (IS61WV51216BLL-10MLI)

I have a use case for communicating with the SDRAM chip onboard the STM32G474E-EVAL1 board.  Took a look at the board schematic https://www.st.com/resource/en/schematic_pack/mb1397-g474e-b04_schematic.pdf and an example project that came with the STM...

mike04_0-1711547479477.png mike04_1-1711547755248.png mike04_2-1711548056794.png mike04_3-1711548266158.png
mike04 by Associate
  • 1499 Views
  • 0 replies
  • 0 kudos

Unable to set HRTIM PWM duty cycle

I am trying to use the HRTIM peripheral on the STM32Hh753VI as a PWM generator with variable duty cycle. I want to use Timer B1 on pin PC8.Firstly, I tried using Simple HAL functions:HAL_HRTIM_SimplePWMStart(&hhrtim, HRTIM_TIMERINDEX_TIMER_B, HRTIM_O...

JTeun.1 by Associate II
  • 4433 Views
  • 4 replies
  • 2 kudos

Resolved! STM32H745 set CM7 boot addr0 from CM4

I'm using a STM32H745 and running a bootloader on the CM4. In the bootloader I want to set the boot address of the CM7 using the user option bytes. Is this possible and if so, how should I do this?Kind regards

Sander-W by Associate
  • 2480 Views
  • 3 replies
  • 0 kudos

I2C Fast Mode Plus, 1 Mb/s

I have an STM32H563 communicating on I2C4 @ 1 MHz (fast-mode plus) to an I/O expander with no problem. However when I add a temp sensor (TI TMP175) to the same bus, communication doesn't work for the TMP175. The TMP175 communicates > 400 KHz only if ...

Resolved! CAN receive doesn't work

Hello everyone, I'm currently doing some experiments with CAN communication with the STM32F302RB Nucleo board. The board is connected to a wcmcu-230 CAN transceiver which is connected to a Raspberry pi with a CAN header connected to it. The bus is te...

JKris17_0-1711367038657.png JKris17_1-1711367110408.png
JKris.17 by Associate II
  • 4758 Views
  • 7 replies
  • 5 kudos

Resolved! FREERTOS, LWIP, HTTPD set up

Hi,Im currently trying to set up a project where Freertos controls a webserver via lwip.I tried following these tutorials/guides and managed to be able to ping the board but not get it to host the webserver.https://github.com/MayaPosch/FreeRTOS_HTTP_...

WilliamVR_0-1710840794056.png WilliamVR_1-1710840885011.png WilliamVR_2-1710840894308.png WilliamVR_3-1710840904622.png
WilliamVR by Associate III
  • 11029 Views
  • 9 replies
  • 4 kudos

Resolved! STM32F103ZE - USB - Login to Windows with the same ComPort

Hello.I have developed a module that has an STM32F103ZE controller. This controller has a USB interface.In order to test the modules, this USB interface is to be connected to a Windows PC via a needle bed. Then various test commands are to be sent vi...

Rassi by Associate II
  • 2277 Views
  • 5 replies
  • 2 kudos