STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SPI Interface

Hello ST expert,I'd like to establish spi communication between my NucleoF401RE and an ADAFruit BLE module.https://www.adafruit.com/product/2633 While waiting for the BLE module, I found a USB SPI converter (like a FTDI for SPI) to create the followi...

Paulo971 by Associate III
  • 2159 Views
  • 1 replies
  • 1 kudos

Resolved! Chosing FLASH for STM32H7

Hello Community,According to data sheet of STM32H743VIT6 https://eu.mouser.com/datasheet/2/389/stm32h743vi-1760857.pdf1) Dual mode Quad-SPI memory interface running up to 133 MHz2) NOR/NAND Flash memory clocked up to 100 MHz in Synchronous mode Q1: I...

Ajaho by Associate III
  • 3256 Views
  • 3 replies
  • 2 kudos

Resolved! Touch sensor with reversed side STM32F429I-DISC1 (touch being detected on the opposite side that was pressed)

Hello.I purchased a Discovery STM32F429-DISC1 development board to start applications involving LCD screen. However, I am having a problem with the touch sensor. I recorded on the board some applications that I developed with TouchGFX, simple applica...

VPatr.2 by Associate II
  • 4045 Views
  • 3 replies
  • 1 kudos

Resolved! Demonstration source code for AN3126

I have been looking into Application Note AN3126 (Audio and waveform generation using the DAC in STM32 products) and in the document a demonstration source code project is mentioned which includes C-language files waveplayer.c and waveplayer.h. I was...

Issue while running debug on STM32G030C8t6

I connected an STM32G030C8T6 to my laptop using ST-link and ran debug using STM32CubeIDE. It was working properly for sometime. But now while putting it on debug, I am getting the following warning message.After this warning message, it does go into ...

Gladson_1-1716022217381.png Gladson_2-1716022325630.png
Gladson by Associate III
  • 1522 Views
  • 1 replies
  • 2 kudos

how to reduce inrush current when stm32 powering up?

Hi,As the title described, how to mitigate the current behavior when stm32 is applied power? My commercial power system are quite sensitive when MCU is power on.For example, let stm32 enters into low power mode once power is on and then control the c...

JKW by Associate III
  • 10976 Views
  • 21 replies
  • 13 kudos

Data-like flash read with memory barrier?

Heyho,I recently finished - or so I thought - the ethernet bootloader for STM32H73x.The bootloader can update the application and vice versa, updating, jumping back and forth, all working fine.Until yesterday all of a sudden (when I was working on so...

LCE by Principal II
  • 8515 Views
  • 22 replies
  • 9 kudos