STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How Do I set a Timer output compare high or low?

I am working on a project that uses a PWM on a timer to drive a buzzer.  When the buzzer stops I need to set the output compare signal high.  The timer set ARR to 250, and the compare value to 125, giving a 4kHz square wave with a 50% duty cycle.   I...

JMala.3 by Associate III
  • 3528 Views
  • 3 replies
  • 0 kudos

stm32h7 ethernet not working

I made several changes in ethernetif.c  pbuf_ref(p); if (HAL_ETH_Transmit_IT(&heth, &TxConfig) == HAL_OK) { while(osSemaphoreAcquire(TxPktSemaphore, TIME_WAITING_FOR_INPUT)!=osOK) { } HAL_ETH_ReleaseTxPacket(&heth); } else { pbuf_free(p); } ////...

Trace on STM32H7

Dear All,I want to use trace on STM32h755So kindly let me know which trace/debugger has to use and what are the pins required. 

vchau.2 by Associate III
  • 1360 Views
  • 1 replies
  • 1 kudos

Resolved! FDCAN2 Rx callback never called (STM32H750)

Hello,On my project, I use FDCAN1 and FDCAN2. FDCAN1 is working perfectly fine.On FDCAN2, I can transmit data successfully (with the CAN ID 0xBEEF), but when I want do receive data, the Rx callback is never called, nor the IRQ handler (the CAN ID fil...

DamienRatazy_0-1719496697177.png

Resolved! ADC

the code generated for my channels if i initialize this channels and    hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2; hadc1.Init.Resolution = ADC_RESOLUTION_12B; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1...

meena_0-1700148308920.png
meena by Associate III
  • 7446 Views
  • 4 replies
  • 0 kudos

Resolved! Complex Bootloader Jump External Flash Application

Hello everyone,I have been working on a custom bootloader for the STM32H735 microcontroller and I am encountering an issue when attempting to jump to my main application stored in external flash memory. Here's a brief overview of what I've done so fa...

HispaEmo_0-1720695797792.png
HispaEmo by Associate III
  • 2030 Views
  • 1 replies
  • 1 kudos

STM32F427 PWM on 40 pins with DMA and BSRR

Hi,I need to generate ~8khz PWM on 40 pins with at least 1% resolution. I was thinking about solution using GPIO ports D,G,F and DMA2 streams 1,2, 7 which are all triggered by TIM8 (TIM8_UP, TIM8_CH1, TIM8_CH4/TRIG/COM).I am worried about the data tr...

Vach23 by Associate
  • 1463 Views
  • 2 replies
  • 0 kudos