STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with external interrupt in PIN B2 stm32h753

Hello,I am working on a project with STM32H753XI mcu and with external interrupts. The problem is that I cannot take an interrupt to PIN PB2. Specifically:1.The Pin is configured as Rising Edge Interrupt (Also tested as falling edge and rising fallin...

SEfte.1 by Associate II
  • 1579 Views
  • 1 replies
  • 0 kudos

Unresolved Inclusion !!

Posted on December 28, 2016 at 07:18Hi,I think you might familiar with  this issue if you are proficient user of Eclipse +STM32.In my #include section of main.c file.Red error line indicates like :(,At the same time the system says to do indexer mar...

0690X00000605t6QAA.png 0690X00000605vaQAA.png

C16 burned in stm32 L010RB

While connecting the battery, the ground was inverted with the VCC and vice versa. As a result, this capacitor burned out. I need to know the function of this part and if I can continue to work normally after what happened. 

IMG_6646.jpeg
Minaihab by Associate III
  • 2614 Views
  • 4 replies
  • 0 kudos

Resolved! stm32f429 ethernet speed control

Hi,I want to make the system with stm32f4 series mcu. An important function of the system is to control the Ethernet speed.Is it possible to adjust the Ethernet speed with such detailed figures as 65Mbps, 38Mbps, and 300Kbps??If possible, how can I a...

inkong by Associate II
  • 4604 Views
  • 4 replies
  • 4 kudos

Resolved! STM32U5A9VJT6Q Power supply requirement

Hi I want to use the STM32U5A9VJ6Q_SMPS inbuilt chip in one of my projects. I plan to run the chip with 3.3V. Is it feasible to run at 3.3V for all pin functions?    

HPK by Associate
  • 1148 Views
  • 1 replies
  • 0 kudos

L4+ detect ff ecc already set

Is there any known way to detect if a double word 0xffffffff value has been programmed? I’m not seeing any quick way, other than finding out after getting flash error bits set. The bootloader I’m working with checks the sector for all 0xff to avoid e...

_EFrie by Senior
  • 2989 Views
  • 5 replies
  • 0 kudos

ADC Conversion Time STM32H563

ADC1 clocked @ 65 MHz, pre-scaler of 8, 7 channels active, 640.5 cycles/conversion, 256 oversampling, interrupts, scan mode. The numbers suggest all channels will be converted 1x in (8/65000000) * 640.5 * 7 * 256 = 141 ms. But when I look at uwTick b...

STM32U5 Flash Write Fails

Hi ,I am writing multiple chunk of each 48 bytes to Flash by following flash programming sequence mentioned in STM32 U5 Reference manual. However some chunks are written properly where some chunks are still remains 0xFF. Please let me know if anybody...

Resolved! How Do I set a Timer output compare high or low?

I am working on a project that uses a PWM on a timer to drive a buzzer.  When the buzzer stops I need to set the output compare signal high.  The timer set ARR to 250, and the compare value to 125, giving a 4kHz square wave with a 50% duty cycle.   I...

JMala.3 by Associate III
  • 3520 Views
  • 3 replies
  • 0 kudos