Skip to main content
Associate III
April 22, 2024
Solved

Identifying Silicon Revision of STM32H735IGK6U

  • April 22, 2024
  • 2 replies
  • 1553 views

Hello,

we are using STM32H735G-DK Eval Boards equipped with differently marked STM32H735IGK6U chips.

One saying:

-------------------

STM32H735

IGK6U

AA126   VQ Z

TWN AA 109

                    D2

--------------------

and the other one saying:

-------------------

STM32H735

IGK6U

AA126   VQ Z

TWN AA 109

                    D3

--------------------

We could not find the meaning of "D2" and "D3" but "D2" is producing HardFaults whereas "D3" is not so we are assuming that these do have different silicon revisions.

 

Could you help us identifying the silicon revision of the chips or what else is "D2" and "D3" standing for?

 

We also attached photos of the different markings.

 

Thank you and best regards

RK_IOT

 

 

This topic has been closed for replies.
Best answer by mƎALLEm

Hello,

The two chips having the same revision rev Z (the latest silicon revision).

You need to contact your local sales for D2 and D3 marking.

2 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
April 22, 2024

Hello,

The two chips having the same revision rev Z (the latest silicon revision).

You need to contact your local sales for D2 and D3 marking.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
April 22, 2024

Both Z step, you can check via DEVID register. 

I think D2/D3 relates to line at plant.

Doubt this is cause of Hard Fault, dig deeper as to WHY it faults.

Likely clocks, power or flash wait states.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..