STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F405 - SPI MPU-6500

Hi,I am trying to communicate with the MPU-6500 from InvenSense and the STM32F405 micro controller in SPI.I managed to read the WHO AM I. And seems to respond well with its value of 0x70.The problem I have is when I want to read the accelerometer and...

Capture d’écran du 2024-08-23 13-42-26.png Capture d’écran du 2024-08-23 13-52-09.png
ELECL.2 by Associate II
  • 3921 Views
  • 4 replies
  • 0 kudos

Resolved! STM32L431 TIM2 Rotary Encoder

Hi, I am having issues using the STM32L431RBI6 to read a rotary encoder.The encoder has a 0-5V output on its 2 channels, and is working with my other STM32 setup (on a STM32L451CCU6).On the STM32L431RBI6, I am using TIM2 configured in Encoder mode, w...

Resolved! STM32H745/755 and STM32H747/757 Bit Banding

I'm writing software on dual core CPU, On M4 core, I need to know is it support bit banding? I searched all documents from ST, but I didn't find clear answer, I found on M4 CPU, like STM32F series bit banding has supported, and on M7 single core CPU ...

Iraj by Associate
  • 2658 Views
  • 2 replies
  • 2 kudos

Resolved! Bootloader DFU on STM32F439ZITx

Hi everyone, I'm developing a bootloader that works like this. I was inspired by the example: https://github.com/pramodk51/bootloader_for_stm32f4.  I developed this initially on Nucleo F439ZI for the test phase and I managed to implement it with the ...

memory_map.png

Resolved! Returning to STM32:: STM32U0 vs STM32L0

Bonjour, (in english below)J'ai travaillé sur un Nucleo-L053R8 de 2015 à 2019 (j'ai encore le Nucleo)Je reprends un travail analogue (réseau d'IoT basse énergie(LE) en milieu agricole, capteurs (certains nécessitant ADC), commandes, petits moteurs .....

Resolved! STM32F439 I2S double the audio frequency

Hi all,I reach out to you all to give some pointers or advice for me where to look into to solve this mystery.I set up my Nuc-STM32F439ZI eval board i2s peripheral to play my audio sine wav file.I used Audacity to generate 13KHz sine wave audio file ...

STM32F429I-Disc1 LCD BSP Issue

Hello, I'm working on a project on the STM32F429I-Disc1 development board and wanted to use the BSP to write characters to the LCD screen. I used STM32CubeMX to configure with LTDC enabled with the default parameters. Since there wasn't BSP configura...

IMG_0225.jpg

USB Device hangs on high data rate in STM32H750VB

I am reaching out to request your assistance with an issue we are encountering on the STM32H750VB microcontroller related to USB data transmission. The problem arises when operating at high data rates, specifically with external USB synchronization a...

Saagar by Associate
  • 1502 Views
  • 1 replies
  • 0 kudos