User Activity

So I am using 2 Nucleo-H563ZI boards, one as controller and the other target, and referencing the knowledge base post "How to set up and run the I3C_Private_Command_IT controller and target example projects." I have a couple questions and issues with...
I am using 2 Nucleo-H563ZI boards, one as controller and the other target, and referencing the knowledge base post "How to set up and run the I3C_Private_Command_IT controller and target example projects" yet I am getting an error. From what I can te...
I have brought down the example I3C_Controller_Private_Command_IT project for the Nucleo-H56ZI, which is the board I am using. When Handle_ENTDAA_Controller(); is executed, it immediately gets to an error that reads "No source available for "<signal ...
I just downloaded the "I3C_Controller_WakeUpFromStop" project for the Nucleo-H563ZI board using the example project import option. It compiled with no issues. Ran it with debugger and protocol analyzer on the I3C bus. When the subroutine "Handle_ENTD...
The project code for my Nucleo-H563ZI sent an I3C Broadcast sequence for dynamic addressing. I can see the Broad cast sequence on the analyzer. There currently is NO I3C Target on to answer, yet the analyzer does show a NACK after RnW(1). I believe t...
Kudos from
Kudos given to