STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Weak SPI clock signal at 12MHz on STM32L4A6ZGT

Below is the analog waveform for the SPI clock at 12MHz. How to improve the strength of this signal and get p-p 3.3V SPI clock at 12MHz ?"GPIO SPEED" set to the "VERY HIGH" setting. Apart from this, is there any additional settings required ? 

STM 12MHz Analog.png

Odd Issue With STM32L071CB When Initialising Watchdog

I'm having an issue with initialising my watchdog, when I include the call to HAL_WWDG_INIT(&hwwdg2) in my code, it is causing any debug attempt to run into the hardfault handler due to some values in SystemClock_Config() being set to 0: __weak HAL_S...

MClarke by Associate II
  • 1958 Views
  • 4 replies
  • 0 kudos

Resolved! Math/FFT Hardware accelerator like the NXP PowerQuad?

Hi there! Are there any plans to add a hardware math accelerator in addition to the cordic and fmac that supports FFT's and other matrix operations entirely in hardware and runs in parallel to the CPU and communicates via DMA? A good example of this ...

etheory by Senior II
  • 3017 Views
  • 3 replies
  • 5 kudos

ADC-DMA buffer value doesn't change

Hi, i have stm32f0c8t6 micro controller. i am using adc-dma with timer interrupt. ADC after working correctly for a while, buffer values doesn't change. what could be the problem?

scotzap by Associate II
  • 979 Views
  • 1 replies
  • 0 kudos

half a USB problem on STM32F401

Hi I designed a replacement pcb for a keyboard of mine with an STM32F401(RCT6).I used the QMK framework to make a firmware which I can download via DFU perfectly fine (I also uploaded it and checked it against what I downloaded..). The PC detects the...

blap by Associate
  • 1795 Views
  • 1 replies
  • 0 kudos

STM32 to StM32 with SPI

I know there are hundreds of posts about this and I've been through most of them but still can't get things to work.The concept is simple: set up 2 Nucleo F446 boards, one as full duplex slave the other as full duplex slave.Master pseudo code:while 1...

Greybeard by Associate II
  • 6166 Views
  • 6 replies
  • 0 kudos

Resolved! External Loader in SPI mode

Hi I am using Stm32L0 series board to create a custom external loader. I am using cubeIDE (version: 1.16.0)I am using winboard W25Q64 chip. I wrote a driver for this chip and interfaced it to my mcu using standard SPI2. I can read /write data on this...

zain_stm32_0-1725837097637.png