Skip to main content
Senior
May 17, 2024
Question

Kit cables

  • May 17, 2024
  • 1 reply
  • 962 views

Hello, got Nucleo F439 kit, amazed to see no cables in it.

Wanted to check if the cable "USB Micro-B connector (CN1)" is same for "USB Micro-AB connector (CN13)" connected in reverse?

Cause Im not able to identify cable "USB Micro-AB" to buy.

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
May 17, 2024

Cables are never included in NUCLEO and DISCOVERY kits because this increases costs and, above all, the amount of waste.

  • A Micro-AB socket accepts both Micro-A and Micro-B plugs and can therefore be used for USB OTG (device or host).
  • A Micro-B socket only accepts Micro-B plugs only and can therefore only be used as a USB device.

Details can be seen in the photos on Wikipedia, for example.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.