STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32h745 Microcontroller Not Responding

I have an STM32H745 Discovery board. The first problem I encountered was when I was creating interfaces using TouchGFX. I could upload them to the microcontroller via the application without any issues, but when I uploaded the code file through C...

motaz9898 by Associate II
  • 2905 Views
  • 7 replies
  • 0 kudos

Resolved! my Nucleo-H755ZI-Q is not programming.

I'm new to microcontrollers. I bought a Nucleo-H755ZI-Q, I connect it to my PC, I make a simple program like turning on and off a LED but the card doesn't do it. I don't know if I have to make any adjustments because it's new.

Resolved! WRITE_REG hard fault

Hallo,I'm compiling with this option   <-fpack-struct=1>Why, with this option, the instruction<WRITE_REG(hdma->Instance->CBR1, 0U);>generates hard fault? I don't understand, without changing nothing.thank you.

IVent.1 by Senior
  • 2471 Views
  • 4 replies
  • 5 kudos

LED won't blink (Timer with PWM)

Hi could somebody please help me with this: i am a beginner ,i have set the Timer_init and Gpio_init with bare Metal i'm working in STM32F429ZIT and i'm aiming to control GPIO pins PG13 and PG14 using the PWM channels with two channel each for every ...

Resolved! Speculation on STM32F767

Hello, I'm studying the STM32F767 MCU, and I noticed that in STMCubeIDE is possible to configure if the speculation is permitted, but I didn't find an explanation of this feature. If I set Speculation disabled, do I set the flash strongly-ordered? Do...

GGran.2 by Associate III
  • 3298 Views
  • 6 replies
  • 3 kudos

Resolved! STM32F429 GPIO 5V tolerant IO behavior

Hello,i use at a STM32F429 the PD5 pin to drive a PNP BJT transistor to switch a sensor supply:PD5 is configured as open drain, and when the stm32 is pulling PD5 low, the transistor supplies the sensor with 5V power. This works so far.But when PD5 is...

scan_ft.png
sk-st by Associate III
  • 4935 Views
  • 8 replies
  • 1 kudos

Resolved! STM32U575 SRAM data retention in Standby mode

 Hello,I am trying to make a program in which the micro stm32u5 is stored in ram memory some data after activating the Sleep Mode.For this I have defined in the flash file the SRAM2 memory that is supposed to be in charge of this and I have saved it ...

Resolved! STM32H753XIH6: issue with pins F1, F2, G2

Hi,I am using STM32H753XIH6 in a new design. The PCB is already manufactured, ready for the assembly. The issue is that I mistakenly designated the pins F1, F2 and G2 as NC in my schematic library model, but realized that the datasheet says they shou...

jd2 by Associate II
  • 1002 Views
  • 1 replies
  • 1 kudos