STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LED Array question

Posted on July 10, 2011 at 21:21I apologize if I am oversimplifying this question, but I'm on the newer side to MCU's.   Anyways, I was trying to figure out putting together a LED array using GPIOC 8-12 and GPIOA 8-12 to make a 4x6 array. I had figu...

how to program a potentiometer

Posted on July 12, 2011 at 09:24hello, I have the STM3210C eval board and there is a potentiometer linked at PC4. I want to divide all the range into ten parts. What should I do ? I have try to do Read Input Data, and all the function ''read...'' pr...

cyril2399 by Associate II
  • 1639 Views
  • 5 replies
  • 0 kudos

STM32F103 in VFQFPN36 with 32.768 kHz RTC crystal?

Posted on July 07, 2011 at 20:04Is it possible for the 36-pin STM32F microcontroller (STM32F103TxU, VFQFPN36 package) to use an external LSE crystal?  Based on the data sheet, it appears to be missing the PC14 (OSC32_IN) and PC15 (OSC32_OUT) pins. T...

stm32f10x_stdperiph_lib warning

Posted on July 10, 2011 at 22:56 In my IAR EWARM version 6.20 STM32 library, both stm32f10x_rcc.c and stm32f10x_dma.c have duplicate #define FLAG_Mask statements, producing a warning at compile time. I redefined the RCC statement and its usage to RC...

Fatal error: Failed to read CPUID for Cortex device

Posted on July 08, 2011 at 08:37I am using Micro controller: STM32F103RCT6TR IDE: IAR Embedded workbench Debugger: J-Link ARM   When I burn it I am getting this error TotalIRLen = ?, IRPrint = 0x..000000000000000000000011 Fatal error: Failed to ...

pradp by Associate II
  • 1790 Views
  • 3 replies
  • 0 kudos

Fatal error: Failed to read CPUID for Cortex device

Posted on July 11, 2011 at 06:33Is this on a board you created, or a commercial eval board? this is the board created not a commercial eval board, I also have a commercial board on which it is working perfect.Check the wiring, and connection, of the...

pradp by Associate II
  • 777 Views
  • 0 replies
  • 0 kudos