STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Motor Control

Posted on July 20, 2011 at 09:32The original post was too long to process during our migration. Please click on the attachment to read the original post.

Simulator for STM32

Posted on July 18, 2011 at 05:18Hi,I am pretty new to STM32 family of controllers. Could you please tell if there is any simulator available for STM32 in IAR Embedded Workbench Version 6.20 and above.RegardsSK

shine by Associate
  • 813 Views
  • 1 replies
  • 0 kudos

[STM32F2xx] FLASH_ProgramOTP implementation?

Posted on July 15, 2011 at 16:16Hello,Going through file stm32f2xx_flash.c, line 620 there is a mention to function FLASH_Status FLASH_ProgramOTP(uint32_t Address, uint32_t Data) but there seems to be no implementation of it ...As there seems to be ...

root by Associate II
  • 923 Views
  • 2 replies
  • 0 kudos

measure time duration

Posted on July 13, 2011 at 09:19I have a string of pulses coming in, and i want to measure the period of a pulse. So i have initialize the input capture for the timer, in my case TIM2 CH4.  RCCIC_Configuration();       /* NVIC configuration */     N...

kong0073 by Associate II
  • 1269 Views
  • 3 replies
  • 0 kudos

STM32F103C8 SPI Not Working

Posted on July 13, 2011 at 20:13Hello -- I'm having no success in getting a clock signal out of the SPI1_SCK pin on our chip.    TIM1 is working as configured.   I've studied the manual,  download materials from the STM web site,  but no further suc...

[HW] pull-up on SWDIO

Posted on July 13, 2011 at 14:26Do I need an external pull-up resistor on the SWDIO line for Serial Wire Debug?The STM32 reference manual (Doc ID 13902 Rev 13) is not quite on this matter… Section 31.4.3: Internal pull-up and pull-down on JTAG pin...

[STM32F205RG] MCU seems to lock itself.

Posted on July 13, 2011 at 13:47Here is the full story ...I re-designed an existing product which was based on a PIC24HJ128GP202 (16 bit, 40 MIPS from Microchip).The new version uses an STM32F205RG (TQFP64).Physically, all JTAG + RST signals are ava...

root by Associate II
  • 2093 Views
  • 4 replies
  • 0 kudos