STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART multiprocessor communication

Posted on May 15, 2010 at 12:21UART multiprocessor communication #lmgtfy #uart-multi-communication #uart-multi-communication #uart-multi-communication #stm32-uart-usart #lmgtfy:-stm32-resources

Kitronix 3.5'',4.3'',7'' TFT LCD with Touch & MCU interface

Posted on June 21, 2011 at 10:42  Kitronix 3.5'', 4.3'' and 7'' TFT LCD modules with Touch Panel & LCD Controller (such as K350QVG-V1-F / K350QVG-V2-F) are provided. They have true TFT LCD colors and 8-bit or 16-bit 8080 system interface and can dir...

sales23 by Associate II
  • 885 Views
  • 1 replies
  • 0 kudos

why cant I get PWM at TIM3 ?

Posted on July 04, 2011 at 19:03void TIM3init(void) {   GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0|GPIO_Pin_1;   GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;   GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;   GPIO_Init(GPIOB, &GPIO_InitStructure...

Select System Clock SYSCLK in system_stm32f10x.c

Posted on July 05, 2011 at 23:43 Hi All, I do not understand the process of frequency selection HSE in the following lines : # if defined ( STM32F10X_LD_VL ) | | (defined STM32F10X_MD_VL ) / * #Define SYSCLK_...

RomainR. by ST Employee
  • 3543 Views
  • 4 replies
  • 0 kudos

IAR flash loader problem

Posted on June 03, 2011 at 11:54hello, I'm working with the lastest version of IAR 6.203, and with a stm32F107 of the steval-pc010v1. I want to load my program and IAr returns the attached file... Is anyone have an idea for solving my problem? Thank...

STM32 virtual com port

Posted on June 05, 2011 at 15:32Hi all, Is there somebody who can give the link for the virtual com port for STM32 device. I didn't find it :(MCU Lüfter