Programming Algorithm
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2009-08-03 11:31 AM
Posted on August 03, 2009 at 20:31
Programming Algorithm
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 4:19 AM
Posted on May 17, 2011 at 13:19
Hi,
I have been working for a while with the Keil development board for the STM32F10x microcontrollers. I have just had some hardware manufactured but required more pins so have used a STM32F103ZC high density micro. I wrote a small test program and managed to program it initially first time. After that though it will not program or erase. I have worked out that the programming algorithm within uvision is for a 512K device. Initially i manually changed the address range within the device options. This caused a long list of errors. I then followed the instructions to write a programming algorithm and added the following code into the project: #ifdef STM32F10x_256 struct FlashDevice const FlashDevice = { FLASH_DRV_VERS, // Driver Version, do not modify! ''STM32F10x High-density Flash'',// Device Name (512kB/384kB/256kB) ONCHIP, // Device Type 0x08000000, // Device Start Address 0x00040000, // Device Size in Bytes (256kB) 1024, // Programming Page Size 0, // Reserved, must be 0 0xFF, // Initial Content of Erased Memory 100, // Program Page Timeout 100 mSec 500, // Erase Sector Timeout 500 mSec // Specify Size and Address of Sectors 0x0800, 0x000000, // Sector Size 2kB (128 Sectors) SECTOR_END }; #endif I followed the instructions to build it, but now it will only load a low density device algorith, and gives an error message saying programming algorithm cannot be found. Any light on this would be very helpful, Thanks very much, CharlieOptions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 4:19 AM
Posted on May 17, 2011 at 13:19
Hello Charlie,
I found a thread in the forum explain the configuration of keil. But for me it didn't work even if I set the correct RAM sizes. I simply chose another, i. e. I chose STM32F103CB when creating the project and then change it to STM32F101CB when compiling. Its not the best solution, but it works fine for me. -Mad