Posted on May 17, 2011 at 13:24It sounds like it might be destructive latch up possibly caused by ESD. Did the fault appear while the card was fitted and not touched or did the fault appear after removing and re-inserting the card. Have you any ESD ...
Posted on May 17, 2011 at 13:23I am using Keil MDK V3 to develop a project based on the STM32F103RDT6 device. I am also using the ST fwr libraries for setting up peripherals. Problem: I have noticed that there are 17 external vectors missing in the ...
Posted on May 17, 2011 at 13:19Can any one explain what the difference is between an 'interupt' and an 'event' in regards to EXTI. I cannot seem to find an explanation in the docs.
Posted on May 17, 2011 at 12:41I am new to the STM32 device and need some help with the ST libraries. I am using the Keil realview MDK which has older ST libraries built in. I have downloaded the latest libraries from ST and unzipped them into 'src'...
Posted on September 13, 2007 at 20:13Does any one know why the cursor position of the Source window and dis-assembly windows are out of sync. I am using the Cosmic compiler 16k limited version V4.5.5 and ST visual dev V 3.3.4 If I place a breakpoint...