STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7S7L8 MCE unable to write

Hello everyone,I'm working on STM32H7S7L8 custom board with same architecture as the DK board ( for XSPIM)The mcu and flash is working fine i can uplaud a boot/appli without issue (touch gfx + lwip work so the hardware is fine)But working on the FW 1...

Hamady_0-1770825023691.png Hamady_1-1770825054492.png Hamady_2-1770825085354.png Hamady_3-1770825107239.png
Hamady by Senior
  • 324 Views
  • 3 replies
  • 0 kudos

Resolved! STM32V8 Series – Datasheet and Nucleo Availability

Hello,ST announced the STM32V8 series some time ago (https://www.st.com/content/st_com/en/campaigns/stm32v8-high-performance-cortex-m85-mcu-z11.html), but there haven’t been any updates since then.I have a couple of questions:How can we download the ...

Fide by Associate
  • 818 Views
  • 1 replies
  • 2 kudos

Resolved! CAN communication between 3 Nucleo boards

Hi, I am trying to establish CAN communication between three different MCUs: NUCLEO-H723ZG, NUCLEO-H755ZIQ, and NUCLEO-G474RE. However, I am unable to successfully communicate between the boards, even though the same baud rate has been configured on ...

Srivatsan_2-1770723670441.png Srivatsan_3-1770723803277.png Srivatsan_0-1770723567676.png Srivatsan_4-1770723922733.png
Srivatsan by Associate III
  • 1613 Views
  • 31 replies
  • 10 kudos

Resolved! AN4879 typo on STM32N6

On AN4879, STM32N6 is marked as Type E (Universal serial bus full-speed host/device interface) But actually it has 2 HS OTG with phy as high-end line up (2* Type D)  

MasterPhi_0-1764151176686.png MasterPhi_1-1764151280384.png

Resolved! STM32U0xx BOR_EN Factory Value

Hi!In version 4 of the reference manual for STM32U0, it is suggested that BOR is enabled and on Level 3 from the factory.Is that correct?I'm currently working on an construction running @ 2V, so it would never start up, if so. And when I read out the...

TSN_0-1770367523381.png
TSN by Associate II
  • 484 Views
  • 9 replies
  • 3 kudos

STM32N6 XIP with Quad spi

We have both a very RAM constrained and space constrained board.  So the OctoFlash chips are larger then i would like.     So being able to XIP off a spi flash that only has 4 SPI lanes would be very helpful.  I just don't know the ramifications of s...

Resolved! STM32H755IIK6 VCAP capacitors placement

Hi, I'm designing the board for STM32H755IIK6. My power supply plan is SMPS + LDO, since I want to use 480MHz speed.  I wonder if there are better recommendations about 2.2uF VCAP placement. There are three VCAP pins, but two 2.2uF capacitors are ins...

mosamasa by Associate II
  • 210 Views
  • 1 replies
  • 0 kudos