STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f103VE enc28j60

Posted on July 27, 2012 at 18:30Hi, I try to connect a enc28j60( ethernet controler) with my stm32f103ve , but all exemples find in web don't work fine. some one to tell an exemple for this? thanks  

Implement USB host for full-speed HID gamepad

Posted on July 25, 2012 at 10:12i was implement USB host for Low-Speed HID gamepad (Discovery board) .... very good. But with gamepad Logitech Full-Speed...it not worki was debug grxsts.b.pktsts ( in interrupt callback USB_OTG_USBH_handle_rx_qlvl_IS...

STM32 Powered through SPI

Posted on July 27, 2012 at 16:10Hello,I have two STM32 chips, one as Master and one as Slave on separate power domains of 3.3V each. My problem is that when the Slave is turned off and power is removed, it is still being powered from the SPI Master....

Popcorn by Associate II
  • 2735 Views
  • 6 replies
  • 0 kudos

BusFault_handler

Posted on July 27, 2012 at 12:42I am trying to communicate STM32F100RB with SD card. Here, I use a code provided by STM for STM32F100VB evolution board. This code contain many functionality like interfacing of Graphics LCD etc. I doesn't need all th...

jai23 by Associate II
  • 1541 Views
  • 1 replies
  • 0 kudos

Change the USART Baudrate !

Posted on July 25, 2012 at 20:37Hello I want to change the USART baudrate in some conditions but i couldn't do this.switch( bdstate)          {            case 0 :              DownloadUsartConfig(9600);              break;            case 1 :      ...

Problem to connect the STM32F4DISCOVERY with ST-Link

Posted on March 24, 2012 at 11:21Hello,I just receive my STM32F4DISCOVERY. I installed IAR EWARM, and ST-Link driver V2. But after several tests on two laptops, I am unable to link the discovery board with ST-Link.This is the message displayed: ''Fa...

NO ST-Link Detected with MDK-ARM

Posted on March 23, 2011 at 08:14Hello, I'm totally novice and need your help. I have installed the lastest version of the MDK-ARM from keil. The result of the compilation is good, but when try to download the programm to the uC, the Software laun...

rgalbany2 by Associate II
  • 6260 Views
  • 12 replies
  • 0 kudos

''No STLink Detected''

Posted on June 27, 2012 at 15:11hi alli am using STM32F407VGT6 Discovery borad, with Keil MDK 4 compiler it was working perfectly, i just update the firmware and when i try to start debugging the updated firmware  Keil MDK shows the notification ''N...

muhammad by Associate II
  • 1949 Views
  • 3 replies
  • 0 kudos