cancel
Showing results for 
Search instead for 
Did you mean: 

3.5'' 320x240 TFT with Touch & LCD controller SSD2119 supporting 8/16-bit 8080, SPI or Parallel RGB interface

sales23
Associate II
Posted on September 21, 2010 at 06:01

3.5' 320x240 TFT with Touch & LCD controller SSD2119 supporting 8/16-bit 8080, SPI or Parallel RGB interface

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
daviddavid92
Associate II
Posted on May 17, 2011 at 14:08

I used the SSD1963 to drive a 480x272 on my design. It works OK, the limitation is the FSMC requiring four cycles per write, thus restricting ultimate graphics speed.

And the documentation is not great.

Chris.

sales23
Associate II
Posted on May 17, 2011 at 14:08

Hello, Chris, If you need any help, please feel free to contact with me. E-mail:

mailto:jacky_sheng@kitronix.com