STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can I use PA11 and PA12 as USB connection ?

Posted on September 06, 2013 at 01:25Guys, I made my own development board with STM32F103VCT6, My question is, How can I use PA11 and PA12 as USB connection ? and how to modify the code from ST, Mass_storage application, so it can be used for my boa...

oscillator sellection

Posted on September 05, 2013 at 16:24hello i designed an eval board base on stm32f107RC myself and i want to program it by using dfu bootloadert then i should download the bootloader file(IAP) from this site so i did this .now do i have to put a 25M...

morykeys by Associate II
  • 2924 Views
  • 6 replies
  • 0 kudos

USART escape sequence and interrupt.

Posted on September 05, 2013 at 18:30Hi,I am usingSTM324x9I-EVAL, which has a 32F439 chip with Keil tools chain and StdPeriph Lib, 1.2RC2, FreeRTOS 7.5.The following is the section of interrupt code.void USART1_IRQHandler(void){  portBASE_TYPE highe...

tonyyu by Associate II
  • 1891 Views
  • 3 replies
  • 0 kudos

Encoder input pulse counting

Posted on September 04, 2013 at 06:10 Hi All, I have a hall effect sensor outputting 0-5V square wave. This is connected to TIM2 CH1 (PA15) on STM32 M4. I am having problems converting this output to RPM value. The output varies from...

stm3220G-EVAL DFU image templet (TASKING)

Posted on September 04, 2013 at 10:39Hi   I'm trying to create a dfu image in TASKING for stm3220G-EVAL. For bootloader I'm using ''STM322xG-EVAL_USBD-FS'' from the STM32_USB-Host-Device_Lib_V2.1.0 library.     The binary templet example in STM32_U...

Frustrating LCD + DMA

Posted on September 04, 2013 at 18:36 Hi :) I'm faced to a DMA who don't want work ... I have look all around (this forum , internet , crystal ball .. ) but i don't know why my screen stay blank :( I use a 320 x 480 (ILI9481) tft scree...

warcatz by Associate II
  • 2167 Views
  • 4 replies
  • 0 kudos

sdio sd card write speed problem

Posted on August 30, 2013 at 03:17hi guys i'm new to stm32, i got a problem that i used sdio and fatfs to test maximum speed of write sd card, its only around 330kb/s but when i try to use sd card reader its up to 2mb/s, so i want to figure out why ...

STM32F415F415RG Unprotect Flash

Posted on September 04, 2013 at 18:14I'm trying to flash a custom bootloader to one of these devices: http://www.mikroe.com/mini/stm32/, and they seem to have protected their bootloader.  I'm using an STM34F4discovery board for SWD, and OpenOCD (0.7...

webbbn by Associate
  • 2449 Views
  • 2 replies
  • 0 kudos