Suspend And Resume Servicing A Pending Timer Interrupt Request
In the M3 Cortex processor world how do I suspend and resume servicing a pending timer interrupt request? In the 8051 world, when the timer overflow the interrupt request flag(TF) is set. If I don't want the timer interrupt service routine to run at the time the request comes in , I would clear the ET flag to stop the interrupt service routine from lanching. Then later when I set the ET flag, the interrupt servie routine would lauch to service the interrupt request (TF). In the Cortex world, what is the equivalent of TF and ET flag. If I clear UIE flag in TIMx_DIER then I will never get a interrupt request. Would it works if set the UIE flag and set the UDIS flag in TIMx_CR1 to suspend the interrupt service routine from lauching? When I clear the UDIS flag would the interrupt service routine launch to service the interrupt request?
Thanks in advance for your help
Ton #i