STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

c write into asm

Posted on November 12, 2013 at 22:41Hi All, please somebody help me to write this c code into asm: void EXTI9_5_IRQHandler(void) {   /* Clear the EXTI line pending bit */   //EXTI_ClearITPendingBit( EXTI_Line8 );   EXTI->PR = EXTI_Line8;   NVIC->I...

STPM01 Data Update Rate

Posted on July 05, 2013 at 15:12Hi,I didnt find nothing in the datasheet refering the data update rate of the calculations that STPM01 do. Do any one knows? I gues that it is 16,66ms but I am no sure.Bye

felipe by Associate II
  • 2629 Views
  • 6 replies
  • 0 kudos

Clocking questions + ccm

Posted on November 11, 2013 at 14:18I have just ported one of my systems over to the STM32F4Discovery board. It is a small OS + TCP/IP. However, I stumbled on a few things: I need to have a 8 khz interrupt for audio sampling. I think I have clocks O...

gullik by Associate II
  • 3162 Views
  • 7 replies
  • 0 kudos

Big data array problem in the STM32F407.

Posted on October 03, 2013 at 21:20Hi Folks We are porting a complex algorithm from the PC into the STM32F407 and we are testing it on a large test file (15000 items long) which I have include in a .h file in the form const int testdataA[15000] = { ...

bl by Associate II
  • 2138 Views
  • 3 replies
  • 0 kudos

USB reports and CRC

Posted on November 08, 2013 at 17:12Hello everyone, I have a product based on an STM32 and a SPI flash NOR memory. I store some data inside the flash NOR, then I read them back through USB. Sometimes (very rare, but happens ..), I get a few corrupte...

Kuikui by Associate III
  • 1660 Views
  • 2 replies
  • 0 kudos

8 bit write on 16 bit wide ext SRAM using NBL0/1

Posted on August 21, 2012 at 04:45Hello, I am have been using an external SRAM with the STM32F207. The SRAM I am using is the Cypress CY62167EV30, a 16-Mbit ( 1M x 16 / 2M x 8 ). The SRAM is used to store a captured image and allow for manipulation...

stbbrad3 by Associate II
  • 1787 Views
  • 2 replies
  • 0 kudos

STM32F4Discovery DSP

Posted on November 11, 2013 at 09:21HiI have a STM32F4Discovery evaluation board. I use CooCox CoIDE and GNU Tools ARM Embedded. While everything works fine if I use standard peripheral library and code, I cannot run anything that is dsp related (li...

peppea82 by Associate II
  • 1963 Views
  • 4 replies
  • 0 kudos

Determining when IWDG has timed out

Posted on November 10, 2013 at 00:52Hi Forum, I need to determine if the IWDG has timed out. After the board resets, can I determine this by checking a flag e.g. if (RCC_GetFlagStatus(RCC_FLAG_IWDGRST) != RESET)   // IWDG has reset or if I know that...

stenasc by Senior
  • 1545 Views
  • 4 replies
  • 0 kudos