2013-06-05 3:05 PM
All my timer interrupts are working except for TIM1. What could be wrong.
I'm using Keil ARM with the STM32F013C8. Here is my startup code: EXPORT WWDG_IRQHandler [WEAK] EXPORT PVD_IRQHandler [WEAK] EXPORT TAMPER_IRQHandler [WEAK] EXPORT RTC_IRQHandler [WEAK] EXPORT FLASH_IRQHandler [WEAK] EXPORT RCC_IRQHandler [WEAK] EXPORT EXTI0_IRQHandler [WEAK] EXPORT EXTI1_IRQHandler [WEAK] EXPORT EXTI2_IRQHandler [WEAK] EXPORT EXTI3_IRQHandler [WEAK] EXPORT EXTI4_IRQHandler [WEAK] EXPORT DMA1_Channel1_IRQHandler [WEAK] EXPORT DMA1_Channel2_IRQHandler [WEAK] EXPORT DMA1_Channel3_IRQHandler [WEAK] EXPORT DMA1_Channel4_IRQHandler [WEAK] EXPORT DMA1_Channel5_IRQHandler [WEAK] EXPORT DMA1_Channel6_IRQHandler [WEAK] EXPORT DMA1_Channel7_IRQHandler [WEAK] EXPORT ADC1_2_IRQHandler [WEAK] EXPORT USB_HP_CAN1_TX_IRQHandler [WEAK] EXPORT USB_LP_CAN1_RX0_IRQHandler [WEAK] EXPORT CAN1_RX1_IRQHandler [WEAK] EXPORT CAN1_SCE_IRQHandler [WEAK] EXPORT EXTI9_5_IRQHandler [WEAK] EXPORT TIM1_BRK_IRQHandler [WEAK] EXPORT TIM1_UP_IRQHandler [WEAK] EXPORT TIM1_TRG_COM_IRQHandler [WEAK] EXPORT TIM1_CC_IRQHandler [WEAK] Then my timer initialization: TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; NVIC_InitTypeDef NVIC_InitStructure; // Enable the TIM gloabal Interrupt NVIC_InitStructure.NVIC_IRQChannel = TIM1_UP_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 2; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); TIM_TimeBaseStructInit(&TIM_TimeBaseStructure); // Time base configuration TIM_TimeBaseStructure.TIM_Period = 1000 - 1; TIM_TimeBaseStructure.TIM_Prescaler = 72 - 1; TIM_TimeBaseStructure.TIM_ClockDivision = 2; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure); // TIM IT enable TIM_ITConfig(TIM1, TIM_IT_Update, ENABLE); // TIM enable counter TIM_Cmd(TIM1, ENABLE); And my interrupt handler: void TIM1_UP_IRQHandler(void) { u16 TID; if(TIM_GetITStatus(TIM1, TIM_IT_Update) == SET) { // Clear timer interrupt flag TIM_ClearITPendingBit(TIM1, TIM_IT_Update); } }2013-06-05 4:24 PM
Is it ticking? Are you using C++?