User Activity

Hello.Reffering to AN4207(Doc ID 023945 Rev 1) Single ended zero reference mode (Page 9):This mode injects an input common mode of half scale to the ADC thus maintaining the dynamic range the same as in differential mode (-32767 to +32767). In this m...
Posted on June 05, 2013 at 07:47Hi! I'm using STM32L152 + IAR6.5. EEPROM writing/erazing routings are placed in RAM. Interrupt vector table and critical interrupt handler too. I need to write EEPROM and serve critical interrupt at the same time. Bef...