STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TIM2 is not generating any interrupts on STM32f051

Posted on December 04, 2012 at 15:56Dear all, I've an issue with TIM2 on the STM32f051 I did a port from STM32f103, however the interrupt is not activated anymore. A big difference is that I use a f0discovery board, so I make use of an internal RC o...

evert2 by Associate II
  • 7327 Views
  • 23 replies
  • 0 kudos

Pulse Lenght

Posted on January 29, 2014 at 14:12I finally managed to setup TIM3 to measure pulse lenght of 4 pwm signal. The only thing left to do is manage the disconnection of one of the wire feeding the signal.For now when the wire is disconnected the last va...

andiob by Associate II
  • 1501 Views
  • 3 replies
  • 0 kudos

New Eclipse STM32L1 Project

Posted on January 29, 2014 at 14:08Hello All!I just got the STM32L1  Discovery board and would like to set up a new project.So far I've been using STM32F103 MCU with the IDE but I used some plugin that already integrated STM32F1 support into Eclipse...

Tom by Associate II
  • 1407 Views
  • 2 replies
  • 0 kudos

Audible DAC/DualModeDMA_SineWave?

Posted on January 29, 2014 at 08:27Guys, I've tried : DAC/DualModeDMA_SineWave/main.c    * @author  MCD Application Team From Standard peripheral library, I can see it already on the osciloscope, how can I make it audible ? How can I adjust the fre...

Delay function on Timer

Posted on January 30, 2014 at 07:43 Hi, I need to implement acculate delay_us. Try to use timer like this. void delay_us ( uint32_t usec ) { TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; /* TIM2 clock enable */ RCC_APB1PeriphC...

suppakit by Associate II
  • 1530 Views
  • 3 replies
  • 0 kudos

problem with updating keil 4.5 to 5

Posted on January 30, 2014 at 05:03i have updated keil 4.54 to 5 when running and compiling same saved project in keil 5 there are some problem and unknown errors!! (i am using rtx kernel) can not open source input file 'RTL.h' no such file or dire...

Using halSleepWithOptions

Posted on January 24, 2014 at 22:49Hi,I'm attempting to put my stm32w108 micro controller to sleep using the halSleepWithOptions function. The comments in halSleepWithOptions suggest calling halPowerDown and halPowerUp before and after waking up fro...

jacobb by Associate II
  • 1598 Views
  • 3 replies
  • 0 kudos

(BTC) Two's complement of ADC input

Posted on January 29, 2014 at 10:24Is it possible to get the 2's compliment of ADC input in STM32F407vg. If It is possible how it can be achieved

sanjib by Associate III
  • 1595 Views
  • 2 replies
  • 0 kudos

ST7735 TFT LCD library for STM32F3

Posted on July 14, 2013 at 05:41I tested a ST7735 TFT LCD with hardware SPI of STM32F3. But I was unable to control the LCD. Are there any implemented library for ST7735 suited to STM32F3 ? Thanks #stm32f3discovery #st7735r