STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32 i2c problem after reciving 3 bytes

Posted on January 31, 2014 at 17:14Hi, I have a problem with i2c interface of stm32f103rbt6 mcu. I use interrupts for sending/receiving data, and everything is ok until slave (MS5611) sent 3 bytes. The bytes are received correctly, but i2c interface...

STM32F4 in package 3 x 3 mm

Posted on January 30, 2014 at 22:24Hi all! The STM32F401 http://www.st.com/web/en/catalog/mmc/FM141/SC1169/SS1577/LN1810?ecmp=ln1810_enews_ln1810_jan2014&sp_rid=NjkwODIzNDM5MTMS1&sp_mid=8196895 contains information about new MCUs in small 3x3mm pack...

ryabokon by Associate
  • 1760 Views
  • 5 replies
  • 0 kudos

stm32 I2c no kommunikation

Posted on November 10, 2011 at 14:38Hi, i try to let two stm32 Boards set all 2 seconds  a few bytes on the general call bus (0x00). Every board allone is doing his job, but when i put them together at the bus, there is nothing going on the I2C bus....

STemWIN + CooCox CoIDE

Posted on September 03, 2013 at 10:47Hello everybody, I would like to try STemWIN library with CoIDE environment. I check that the examples only for the payed license tools. I try set up the CoiDE project but I've linker errors.        [cc] c:/progr...

totti001 by Associate II
  • 4178 Views
  • 9 replies
  • 0 kudos

.NET Micro Framework for 429iDiscovery

Posted on January 28, 2014 at 15:23Hi everybody.I just downloaded and flashed .NET Micro Framework provided by ST, at link http://www.st.com/web/en/catalog/tools/PF260087 (UM1676).Board boots fine, bu after having installed USB Driver (after having ...

maiorfi by Associate II
  • 1152 Views
  • 1 replies
  • 0 kudos

Problem with DMA

Posted on January 23, 2014 at 06:12The original post was too long to process during our migration. Please click on the attachment to read the original post.

sanjib by Associate III
  • 5065 Views
  • 13 replies
  • 0 kudos

RTX interrupt configuration

Posted on January 31, 2014 at 09:36Hello,I'm using STM32l152-discovery and  trying to configure interrupt on usart2 while using RTOS Keil RTX, but I can't find any info about RTX interrupt configuration. Should i configure them the same way as I do ...

k_ by Associate II
  • 761 Views
  • 0 replies
  • 0 kudos

STM32F3 CCM RAM WITH CoIDE

Posted on January 29, 2014 at 14:50I`m trying to configure a STM32F3 Project with the CoIDE 1.7.6 to run an ISR from CCM RAM basing on the AN4296 application note, but I can't put it to work with the CoIDE.

Asantos by Senior
  • 954 Views
  • 2 replies
  • 0 kudos

Reading voltage -ADC

Posted on February 27, 2012 at 11:29hi.. I'm using STM32 VL microcontroller.I need to read voltage continiously..so i'm using timer 2 in interupt mode to read ADC value.below is my code.. wheneven ADCread value function is colled from TIM2 interrupt...

mayakk12 by Associate II
  • 8409 Views
  • 27 replies
  • 0 kudos