cancel
Showing results for 
Search instead for 
Did you mean: 

Timer Set up conf: intriguing issue.

bl
Associate II
Posted on May 20, 2013 at 16:04

Hi Folks 

I have this simple example program that I am modifying and by moving one statement into a while statement it breaks it. I'm working on the STM32F4 Discovery board

Here is the code:- 

/*

 ===============================================================================

 Name        : main.cpp

 Author      : 

 Version     :

 Copyright   : Copyright (C)

 Description : main definition

 ===============================================================================

 */

&sharpifdef __USE_CMSIS

&sharpinclude ''stm32f4xx.h''

&sharpendif

&sharpinclude <stdio.h>

/* Private typedef -----------------------------------------------------------*/

GPIO_InitTypeDef GPIO_InitStructure;

TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

/* Private define ------------------------------------------------------------*/

/* Private macro -------------------------------------------------------------*/

/* Private variables ---------------------------------------------------------*/

/* Private function prototypes -----------------------------------------------*/

void

LED_Config(void);

void

INTTIM_Config(void);

/* Private functions ---------------------------------------------------------*/

/**

 * @brief  Main program

 * @param  None

 * @retval None

 */

int

main(void)

{

  /* LED Configuration */

  LED_Config();

  INTTIM_Config();

  while (1)

    {

      //INTTIM_Config();

      while (TIM_GetFlagStatus(TIM2, TIM_FLAG_Update ) == RESET)

        {

        };

      TIM_ClearFlag(TIM2, TIM_IT_Update );

      GPIO_ToggleBits(GPIOD, GPIO_Pin_13 );

    }

}

/**

 * @brief  Setup an interval timer

 * @param  None

 * @retval None

 */

void

INTTIM_Config(void)

{

  /* TIM2 clock enable */

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);

  /* Time base configuration */

  TIM_TimeBaseStructure.TIM_Period = 200 - 1; // 1 MHz down to 10 KHz (0.1 ms) between 0x0000 and 0xFFFF.

  TIM_TimeBaseStructure.TIM_Prescaler = 134 - 1; // 24 MHz Clock down to 1 MHz (adjust per your clock)  between 0x0000 and 0xFFFF

  TIM_TimeBaseStructure.TIM_ClockDivision = 0;

  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

  TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);

  /* TIM2 enable counter */

  TIM_Cmd(TIM2, ENABLE);

}

void

LED_Config(void)

{

  /* GPIOD Periph clock enable */

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);

  /* Configure PD12, PD13, PD14 and PD15 in output pushpull mode */

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14

      | GPIO_Pin_15;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_Init(GPIOD, &GPIO_InitStructure);

}

As it stands the code works fine - however if I commit out the active INTTIM_Config() and make the INTTIM_Config() in the loop active the time base init does not work and the timer stays at default values. 

Any thoughts welcome.

CS

#timer-set-up-stm32f4
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on May 20, 2013 at 23:57

I'm not sure why you are surprised by this behaviour. After the initialization, all the timer flags are likely cleared. Therefore it would never enter the inner while{} loop. Once you complete the outer/main while loop, you re-initialize the timer, resetting its counter value, clearing flags etc. Of course your LED should toggle - very quickly probably!

bl
Associate II
Posted on May 21, 2013 at 10:44

Hi Finkelmeyer

I think I understand what you are saying, however why on the first loop does it not work if the INTTIM_Config(); is inside the while(1) statement. 

In the working case (first time) it executes INTTIM_Config(); then  while(1) and then even thing is fine, however in the second case it executes while(1) then INTTIM_Config(); and the values are not loaded. 

This morning I tried running a number of  INTTIM_Config(); outside the loop to see if that would break it - but it didn't. 

So next I'm going to simulate a number of the loops with in line code to see what happens. 

CS

bl
Associate II
Posted on May 21, 2013 at 12:42

Hi Folks 

Interestingly this looks like a timing issue, if I change the loop code to 

  while (1)

    {

      INTTIM_Config();

      int i = 0;

      while (i < 1000)

        {

          i++;

        };

          while (TIM_GetFlagStatus(TIM2, TIM_FLAG_Update ) == RESET)

            {

            };

          TIM_ClearFlag(TIM2, TIM_IT_Update );

          GPIO_ToggleBits(GPIOD, GPIO_Pin_13 );

        }

This works, however if I change it to ''while (i < 100)'' it breaks, so it shows there needs to be a time between setting up the timer and using it. Probably some parrellalism going on in the compiler, which is flushed by the 'while' statement. 

..Mmm interesting!!

yuvanelex
Associate
Posted on May 21, 2013 at 13:48

Hi are you try for the Channel 3 and 4 of timer 2...?