Samsung 128Mbytes NAND flash ?
Posted on February 14, 2014 at 13:17Guys Does anyone know where I can find a library for 128Mbytes NAND flash from Samsung ? thanks for the info
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on February 14, 2014 at 13:17Guys Does anyone know where I can find a library for 128Mbytes NAND flash from Samsung ? thanks for the info
Posted on February 15, 2014 at 21:53This software is not working with STM32F030K6 , but this sofware works with STM32F030R8. Prototype 1 used the discovery board. No we made a PCB with STM32F030K6. And the code is not working anymore. Makes reset. ...
Posted on January 23, 2013 at 07:03Hi, Yesterday i have taken a STM32W RFC kit, in the user manual of RFC kit in section 1.8.2 it is given that ''To use the serial communication channel on the kit application boards, a Virtual COM port driver for S...
Posted on February 16, 2014 at 23:00I'm planning a prototype using HID and coOS, using coIDE, and would like to know if somebody tried before those products together.Thanks in advance. Best regards. #go-to-the-horse's-mouth
Posted on February 13, 2014 at 08:48Hello, I use a STM32F405 in a design. I have a test softaware for the board to ttest GPIOs, CAN,...) It was working well, but suddenly nothning work at all (also functions that was working before). I try to reflas...
Posted on February 16, 2014 at 21:24 Hello Based on some examples on the forum, here (Thank you). I am using the STM32F407 based discovery board. I have the following code that works fine, but PA2, PA3, and PC4 do not give me the...
Posted on September 12, 2012 at 08:57Hi! I've got another problem with my STM32F205. The Data Timeout timer doesn't start and when there is no answer from SD Card, the system waits in loop for watchdog reset ;). Here is a function. The code is wor...
Posted on February 17, 2014 at 06:40Dear All, I am looking to generate short pulses (1us) for an application. On first appearance, the datasheet looks to be very imprecise as to the shortest pulse that can be generated, i.e.:''Pulse lengths and wav...
Posted on February 14, 2014 at 15:33Hi,I'm working with stm32F0 and I want read ADC multichannel. My question is: is it possible without DMA?Thanks
Posted on January 11, 2014 at 10:45Hello,I've been spending some time looking through the STM32F4 reference document and it looks quite clear that the I2S2 / I2S2ext are supposed to be used in a full-duplex configuration.However, I'm curious, is it ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.